MPXV5004G sensitivity and error percentage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPXV5004G sensitivity and error percentage

689件の閲覧回数
a1
Contributor I

I'm using the MPXV5004G pressure sensor.  I wish to record

sensitive changes in my breathing.  I hooked it up to a

10-bit analog to digital converter and typical breathing is

moving the output value maybe 1 point at best.

I wish to amplify the sensitivity, but I notice that the

MPXV5004G has error of 1.5% or 2.5%.  This seems to say

that the output value error is greater than 1 point out of

1024 values, so even if I amplified the changes, could I

trust them?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)