MPXV5004DP vs MPXV5004GC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPXV5004DP vs MPXV5004GC

541件の閲覧回数
cram1
Contributor I

could we use these sensors for measuring negative pressure of -2kPa?

ラベル(1)
0 件の賞賛
1 返信

450件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello Marc,

The MPXx5004 family have a pressure range from 0 to 3.92kPa and not suitable for negative pressure readings as per the sensor can get damaged.

If you need to measure negative values of -2kPa or higher, we recommend the vacuum sensors below:

  • MPXV7002 family with a pressure range of -2 to 2kPa
  • MPXV7007DP differential and gauge pressure sensor with a pressure range of -7 to 7 kPa
  • MPXV70025DP differential and gauge pressure sensor with a pressure range of -25 to 25kPa

I hope this information can be helpful.


Have a great day,

Paulina

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛