MPXH6300A6U, a defective part or not?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPXH6300A6U, a defective part or not?

249 次查看
Jeffreylee1
Contributor I

MPXH6300A6U

 

Hello. I purchased this part from Mouser.

This image is the part called MPXH6300A6U and taken by microscope.

There is a hole in the middle of the part and you can see inside the bottom a thin layer or coating.

It seems like, in the layer or coating, there is a little bubble? some flaw? something like that.

Could you check this is okay? Could you guarantee this is not a defective part?

0 项奖励
1 回复

238 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jeff,

from the first look the Gel inside the sensor looks ok to me. The particles look like dust on the top of the Gel. You cannot avoid to get dust particles to lay on top of the Gel as the hole is not covered. 

JozefKozon_0-1707805197976.png

The Gel on the top of the the silicon Die is applied under vacuum to avoid any bubbles creation in the Gel. If you see any bubbles in the Gel, then it is definitely wrong and you can return the components under warranty, but from the picture under the microscope you sent it looks like dust particles, so the components are ok. 

JozefKozon_1-1707805408479.png

You can test the components. Apply a pressure to the pressure sensor under the conditions stated in the datasheet and if you measure the correct output voltage +/-error stated in the datasheet, then the sensor is working correctly. If the error is higher, then you can apply for CQI (Customer Quality Incident) and NXP will check if the components are faulty. But I don't expect any problems based on the data you shared.

JozefKozon_2-1707805749881.png

 

With Best Regards,

Jozef

 

0 项奖励