MPXA6115AC7U (vacuum sensor) for the vacuum packing machine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPXA6115AC7U (vacuum sensor) for the vacuum packing machine

812 Views
Younghyun
Contributor I

Hi, 

 

I am considering using this sensor, MPXA6115AC7U (vacuum sensor) for the vacuum packing machine in terms of reliability because the machine is the product to sell.

Can it be reliable the conditions below? 
- Vacuum conditions: 0 to -110 KPa in 20sec. for many many times (several hundred times) continuously during daily working time. 

 

 
Tags (1)
0 Kudos
1 Reply

807 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Younghyun Kim,

the MPXA6115AC7U is capable to measure the pressure from 15kPa to 115kPa. As long as the values will not exceed the maximum values in the Table 2. in the MPXxx6115A datasheet, the sensor will work reliably.

 

JozefKozon_1-1646384812901.png

Please note, that the MPXA6115AC7U is not capable to measure pressure from 0kPa to 15kPa. If applied pressure is lower or equal, than 15kPa and above or equal, than 0kPa the output voltage will not change. Please refer to Figure 5. in the MPXxx6115A datasheet.

JozefKozon_2-1646384833904.png

With Best Regards,

Jozef

 

0 Kudos