MPX5700DP/MPX5500DP - Way to detect connected sensor (maybe using V1, V2 and Vex pins?)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPX5700DP/MPX5500DP - Way to detect connected sensor (maybe using V1, V2 and Vex pins?)

668 Views
CVi
Contributor I

Hi,

I wander if is it possible to hardware-detect which of the two MPX5700DP / MPX5500DP sensors is mounted on the board.

Can I use the V1, V2 and Vex pins with some circuitry between the sensor and the MCU to detect which sensor is connected? If yes, how? What type of signals are them?

I found in other questions (1, 2, 3) that those pins must be leave not connected.

But is there any possibility to use them for this scope, please?

Thank you in advance.

 

Bye,

Clem

0 Kudos
Reply
2 Replies

639 Views
CVi
Contributor I

Ok, Tomas, thank you anyway.

Best regards,

Clemente

0 Kudos
Reply

648 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Clemente,

I am afraid there is no way to use these pins for this purpose and I cannot think of any other suitable possibility to achieve that, unfortunately.

Best regards,

Tomas

0 Kudos
Reply