MPX4115AP weird reading

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPX4115AP weird reading

ソリューションへジャンプ
3,638件の閲覧回数
Ghost13
Contributor I

I have the MPX4115AP sensor. I have it hooked up according to you datasheet. The output of Pin 1 (Pin 3 is +5V) starts at 3.8V when power is first applied, and then drops gradually to about 2.5V after 5-10 seconds. The air pressure is not changing.
When I do change the air pressure, however, the reading continues to drop - it has no effect.

Any help would be appreciated (and the sooner the response the better)!

Thanks!!!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,631件の閲覧回数
Joshevelle
Senior Contributor I

Hello Mark,

Yep, you're rigth... I'll ask the appropriated persons to take a look at the dates on the forums. Perhaps Carlos might help 4guin4g4 ?

Well, at least he had an answer from us =).

Cheers,

Josh

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,631件の閲覧回数
Joshevelle
Senior Contributor I

Hello Ian,

Could you please let me know what is the specific part number of the device that you're using? There are two datasheets for this device (depending on the device version), both of them shows the pin out as follows:

pin#1: NC

pin#2: Vs

pin#3: GND

pin#4: Vo

       

MPXAZ4115A Series:

http://cache.freescale.com/files/sensors/doc/data_sheet/MPXAZ4115A.pdf

MPXV4115V Series:

http://cache.freescale.com/files/sensors/doc/data_sheet/MPXV4115V.pdf

Regards,

Josh

0 件の賞賛
返信
2,631件の閲覧回数
rocco
Senior Contributor II

Hi Josh,

Something is wrong with the dates on this board. I believe Ian asked that question more than 5 years ago.

The board shows he asked the question on October 1 of this year, but that Alban responded back in 2007. The June 2007 date is correct, so I would hope that Ian is not still waiting on an answer.

0 件の賞賛
返信
2,632件の閲覧回数
Joshevelle
Senior Contributor I

Hello Mark,

Yep, you're rigth... I'll ask the appropriated persons to take a look at the dates on the forums. Perhaps Carlos might help 4guin4g4 ?

Well, at least he had an answer from us =).

Cheers,

Josh

0 件の賞賛
返信
2,631件の閲覧回数
4guin4g4
Contributor IV

I will take a look at the migration of the dates..

0 件の賞賛
返信
2,631件の閲覧回数
Ghost13
Contributor I
No suggestions?!?!?!
:smileysurprised: :smileysad: :smileymad:
:smileyindifferent:
0 件の賞賛
返信