MPX2202GP Pressure transducer maximum gauge pressure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPX2202GP Pressure transducer maximum gauge pressure

655 Views
abinm100
Contributor I

Hi,

I am looking at the specifications of the MPX2202GP pressure transducer and it says that the absolute pressure range is 20 kPa to 200 kPa. Does it mean that for gauge pressure (at atmospheric pressure), the maximum value of the sensor is 100 kPa?

Thank you for your help.

Regards,

Azim

0 Kudos
1 Reply

606 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Azim,

The MPX2202A (absolute type) measures an external pressure relative to a pressure reference (vacuum) sealed inside the reference chamber of the die during manufacture. Its minimum operating pressure is 20kPa and maximum 200kPa.

 

The MPX2202G (gauge type) measures the difference between pressures applied simultaneously to opposite sides of the diaphragm. Typically an ambient atmospheric pressure is applied to the “P2” side through the vent hole in the chip of the differential pressure sensor element. Then the maximum pressure the MPX2202G can measure is 200kPa above the ambient atmospheric pressure.

Best regards,

Tomas

0 Kudos