MPX2202GP Pressure transducer maximum gauge pressure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPX2202GP Pressure transducer maximum gauge pressure

709 次查看
abinm100
Contributor I

Hi,

I am looking at the specifications of the MPX2202GP pressure transducer and it says that the absolute pressure range is 20 kPa to 200 kPa. Does it mean that for gauge pressure (at atmospheric pressure), the maximum value of the sensor is 100 kPa?

Thank you for your help.

Regards,

Azim

0 项奖励
1 回复

660 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Azim,

The MPX2202A (absolute type) measures an external pressure relative to a pressure reference (vacuum) sealed inside the reference chamber of the die during manufacture. Its minimum operating pressure is 20kPa and maximum 200kPa.

 

The MPX2202G (gauge type) measures the difference between pressures applied simultaneously to opposite sides of the diaphragm. Typically an ambient atmospheric pressure is applied to the “P2” side through the vent hole in the chip of the differential pressure sensor element. Then the maximum pressure the MPX2202G can measure is 200kPa above the ambient atmospheric pressure.

Best regards,

Tomas

0 项奖励