Dear All,
One of my customer wants develop a touchpad for their end product. Below is the customer requirement.
1. 4 Touch Pad
2. 4 LED Indication
3. I2C interface for host processor
I'm promoting MPR121 and have made a rough schematic for total BOM conclusion. Please review my schematic and suggest if any changes needs to be done.
Thanks in advance
Regards
Mithun
FAE
WTMEC
已解决! 转到解答。
Mithun,
Looks fine, just a few comments:
1. As VDD is higher than 2.75V, the VDD and VREG pins should not be connected together. Use a separate 0.1μF decoupling ceramic capacitor on VREG to VSS as shown in figure 2 of the datasheet.
2. In the final schematic, do not forget to connect the ADDR pin accordingly.
3. If the customer is going to use the IRQ output, use a level translator also on this line. I do not have much experience with discrete MOSFETs, I usually use an integrated solution such as the PCA9306DCUR from TI.
Regards,
Tomas
Mithun,
Looks fine, just a few comments:
1. As VDD is higher than 2.75V, the VDD and VREG pins should not be connected together. Use a separate 0.1μF decoupling ceramic capacitor on VREG to VSS as shown in figure 2 of the datasheet.
2. In the final schematic, do not forget to connect the ADDR pin accordingly.
3. If the customer is going to use the IRQ output, use a level translator also on this line. I do not have much experience with discrete MOSFETs, I usually use an integrated solution such as the PCA9306DCUR from TI.
Regards,
Tomas
Hi Mithun,
Two comments:
1. Both PTA2 (SDA) and PTA3 (SCL) pins are used for I2C communication, so you cannot use them to drive LED3 and LED4. Use PTB4 and PTB5 pins to drive these LEDs.
2. In the final schematic, do not forget to connect a crystal or ceramic resonator to the XTAL and EXTAL pins as shown in Figure 2-7 of the MC9S08PT16 Reference Manual, unless you make use of the internal reference within the MC9S08PT16.
Regards,
Tomas