Is there a block diagram for the pin structure of the INT pins? Are they OD or totem pole? If there are internal PU/PD resistors what are the values?
I am trying to understand if there is a backfeed path from INT1 or INT2 back to VDD or VDDIO when VDD/VDDIO are high impedance and there is an external voltage on INT1 or INT2.
What kind of current can be tolerated in this condition?
解決済! 解決策の投稿を見る。
Hello Terry,
The INT pins can be configured using the PP_OD bit to be push-pull (PP_OD = 0 - default) or open drain (PP_OD = 1).
The polarity of the INT pins can be configured using the IPOL bit. The default value is active low (IPOL = 0) meaning any interrupt event is signaled with a logical 0.
PS: Note that the MMA8451QR1 is in “End of Life” status and we recommend either the FXLS8974CF or FXLS8967AF as a replacement.
BR, Tomas
Hello Terry,
The INT pins can be configured using the PP_OD bit to be push-pull (PP_OD = 0 - default) or open drain (PP_OD = 1).
The polarity of the INT pins can be configured using the IPOL bit. The default value is active low (IPOL = 0) meaning any interrupt event is signaled with a logical 0.
PS: Note that the MMA8451QR1 is in “End of Life” status and we recommend either the FXLS8974CF or FXLS8967AF as a replacement.
BR, Tomas