hi,i want use MMA8451Q to detect move and init it as
bool MMA8451Q_Init(void){
unsigned char val;
/* Place the MMA8451Q in sleep mode,ODR 100HZ */
MMA8451Q_WriteReg(0x2A,0x18);
/* motion detection,enable XYZ */
MMA8451Q_WriteReg(0x15,0xD8);
/* set threshold */
MMA8451Q_WriteReg(0x17,0x08);
MMA8451Q_WriteReg(0x18,0x0A);
/* enable motion dection interrupt */
MMA8451Q_WriteReg(0x2D,0x04);
/* set interrupt pin */
MMA8451Q_WriteReg(0x2E,0x04);
#if 0
/* Set on-board Acc sensor range to 8G */
MMA8451Q_WriteReg(0x0E,0x02);
#endif
val = MMA8451Q_ReadReg(0x2A);
MMA8451Q_WriteReg(0x2A,val | 0x01);
/* Acc sensor WHO_AM_I check... */
if (0x1A == MMA8451Q_ReadReg(0x0D)){
MMA8451Q_GpioIntInit();
return true;
}else{
return false;
}
}
after init ,i read some of reg and print as follow
Reg addr <--> val
Reg 0x09 <--> 0x00
Reg 0x0a <--> 0x00
Reg 0x0b <--> 0x01
Reg 0x0c <--> 0x00
Reg 0x0d <--> 0x1a
Reg 0x0e <--> 0x00
Reg 0x0f <--> 0x00
Reg 0x10 <--> 0x00
Reg 0x11 <--> 0x80
Reg 0x12 <--> 0x00
Reg 0x13 <--> 0x44
Reg 0x14 <--> 0x84
Reg 0x15 <--> 0xd8
Reg 0x16 <--> 0x00
Reg 0x17 <--> 0x08
Reg 0x18 <--> 0x0a
Reg 0x1d <--> 0x00
Reg 0x1e <--> 0x00
Reg 0x1f <--> 0x00
Reg 0x20 <--> 0x00
Reg 0x21 <--> 0x00
Reg 0x22 <--> 0x00
Reg 0x23 <--> 0x00
Reg 0x24 <--> 0x00
Reg 0x25 <--> 0x00
Reg 0x26 <--> 0x00
Reg 0x27 <--> 0x00
Reg 0x28 <--> 0x00
Reg 0x29 <--> 0x00
Reg 0x2a <--> 0x19
Reg 0x2b <--> 0x00
Reg 0x2c <--> 0x00
Reg 0x2d <--> 0x04
Reg 0x2e <--> 0x04
Reg 0x2f <--> 0x00
Reg 0x30 <--> 0x00
Reg 0x31 <--> 0x00
iic work OK,and reg value is right,but i can't recv any interrupt signal from MMA8451Q.
i read reg 0x0C(INT_SOURCE) in a dead loop and print it,it always is 0x00.
can you help me?
Hello,
Thank you for writing.
In order to configure the MMA8451Q in Motion Detection mode, I suggest using the following configuration:
unsigned char reg_val = 0;
I2C_WriteRegister(MMA845x_I2C_ADDRESS, CTRL_REG2, 0x40); // Reset all registers to POR values
do // Wait for the RST bit to clear
{
reg_val = I2C_ReadRegister(MMA845x_I2C_ADDRESS, CTRL_REG2) & 0x40;
}while (reg_val);
I2C_WriteRegister(MMA845x_I2C_ADDRESS, XYZ_DATA_CFG_REG, 0x02); // +/-8g range
I2C_WriteRegister(MMA845x_I2C_ADDRESS, CTRL_REG1, 0x18); // ODR = 100Hz, Standby mode
I2C_WriteRegister(MMA845x_I2C_ADDRESS, FF_MT_CFG_REG, 0x58); // Motion detection for X and Y axis
I2C_WriteRegister(MMA845x_I2C_ADDRESS, FT_MT_THS_REG, 0x08); // Threshold Setting Value for the Motion detection (0.5g)
I2C_WriteRegister(MMA845x_I2C_ADDRESS, FF_MT_COUNT_REG, 0x05); // Set the debounce counter to 50 ms timer (50ms)
I2C_WriteRegister(MMA845x_I2C_ADDRESS, CTRL_REG4, 0x04); // Enable Motion/Freefall Interrupt
I2C_WriteRegister(MMA845x_I2C_ADDRESS, CTRL_REG5, 0x04); // Motion/Freefall interrupt routed to INT1 - PTA14
reg_val = I2C_ReadRegister(MMA845x_I2C_ADDRESS, CTRL_REG1); // Put the device in active mode
I2C_WriteRegister(MMA845x_I2C_ADDRESS, CTRL_REG1, reg_val | 1);
In case you need more details about the Auto-WAKE/SLEEP mode, I recommend the following post:
https://community.nxp.com/docs/DOC-332453
Please let me know if you have any further question about the code mentioned above.
Best Regards,
David