MMA8451Q interrupt read mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMA8451Q interrupt read mode

681件の閲覧回数
maurogatti
Contributor I

Hello.

I configured the MMA8451Q with ODR = 800Hz, so I can read the acceleration's components with a 1,25 ms  sample period.

The  polling mode is ok, I can do a read with  800Hz sample frequency.

But I can do it in "interrupt mode" (I configured MMA8551 as described in AN4076) because I see the interrupt pulse every 24 ms (about 40 Hz).

Why? 

Thanks

ラベル(1)
0 件の賞賛
1 返信

414件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Mauro,

Thank you very much for writing.

In this case, I highly recommend to use the sample project from the link below as a reference for your application:

https://community.nxp.com/docs/DOC-98836 

Please note that in the project, the interrupt mode is used.

Please let me know if you have any further question and I will be glad to help you.

 

Best Regards,

David

0 件の賞賛