MAG3110 reliability under strong magnetic flux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MAG3110 reliability under strong magnetic flux

跳至解决方案
1,522 次查看
ble
Contributor I

Hello,

I am developing a device with MAG3110 magnetometer. It will be used in an area with strong magnetic flux.

I wondered whether it will shorten the life of the MAG3110 or should I expect it to work fine for the normal life of the MAG3110? (Which is how long?)

Thanks

标记 (1)
0 项奖励
1 解答
1,247 次查看
Joshevelle
Senior Contributor I

Hello Ariel,

The sensor would not be damaged as long as you don't exceed the maximum magnetic field it can support (100,000uT). Since the life spam of the device would depend on the customer application, we do not have an estimate of life.

I highly recommend you to take a look at the following application note, which describes how to calibrate the MAG3110 in the presence of hard and soft iron interference:

http://cache.freescale.com/files/sensors/doc/app_note/AN4246.pdf

Hope it helps!

Josh

在原帖中查看解决方案

0 项奖励
1 回复
1,248 次查看
Joshevelle
Senior Contributor I

Hello Ariel,

The sensor would not be damaged as long as you don't exceed the maximum magnetic field it can support (100,000uT). Since the life spam of the device would depend on the customer application, we do not have an estimate of life.

I highly recommend you to take a look at the following application note, which describes how to calibrate the MAG3110 in the presence of hard and soft iron interference:

http://cache.freescale.com/files/sensors/doc/app_note/AN4246.pdf

Hope it helps!

Josh

0 项奖励