LF Antenna Part Suggesion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LF Antenna Part Suggesion

Jump to solution
255 Views
Pranav_Tonape
Contributor I

Dear NXP,

We are working on TPMS RF Project. with NXP part NTM88H135ST.

 
In this project we are using B82450A1084C000 transponder coil for LF Communication.

1) can you please suggest us is this part suitable with NXP NTM88H135ST1 IC or not ?

2) if not then can you suggest any other alternative/suitable part for LF communication?

 

thanks and regards,

Pranav Tonape.

0 Kudos
1 Solution
240 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Pranav,

We do not recommend this LF coil for proper operation of the LFR.

The sensitivity is too low (3.4mV/µT), leading to a too much reduced voltage at the input of the device.

On our reference design we use the B82450A7204A000 (7.2mH) with a much higher sensitivity (52mV/µT) at the penalty of an increased size (11.4mm vs 3.2mm).

Otherwise, I think a good trade-off could the B82450A1855E001 (18.52mH) with a sensitivity at 50mV/µT and a length of 7.8mm.

BR, Tomas

 

View solution in original post

0 Kudos
1 Reply
241 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Pranav,

We do not recommend this LF coil for proper operation of the LFR.

The sensitivity is too low (3.4mV/µT), leading to a too much reduced voltage at the input of the device.

On our reference design we use the B82450A7204A000 (7.2mH) with a much higher sensitivity (52mV/µT) at the penalty of an increased size (11.4mm vs 3.2mm).

Otherwise, I think a good trade-off could the B82450A1855E001 (18.52mH) with a sensitivity at 50mV/µT and a length of 7.8mm.

BR, Tomas

 

0 Kudos