KL27 & KL47 Support for Sensor boards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL27 & KL47 Support for Sensor boards

640 Views
marcocesar-a211
NXP Employee
NXP Employee

Is there a way to use KL27 or KL47 Freedom boards with the Freedom Senso Toolbox boards?  (ie. AGM01 and MULTI-B)

Labels (1)
0 Kudos
1 Reply

374 Views
michaelestanley
NXP Employee
NXP Employee

Marco,

Out of the box projects are supported only for KL25Z, KL26Z, KL46Z, K20D50M and K64F.  These collectively cover ARM Cortex M0+, M4 and M4F processor types, and are intended to act as "reference designs" for other ports.  I haven't studied the schematics for the KL27 and KL47, but I would be very surprised if they coundn't be used.  Hardware resources required by the fusion kit are minimal, and include I2C, UART and GPIO to drive LEDs.  These are easily mapped in Processor Expert and the process is outlined in the user guide included in the docs directory with the kit.  The precanned KL26Z and KL46Z projects are your best reference points.  I would even go so far as to purchase one of those two boards as well so that you can use the canned projects as a sanity check.

Good luck and have fun!

Mike

0 Kudos