Hi - Does the MPH6250A6T1 pressure sensor come with any options to protect (seal) the port opening during the assembly process (i.e. aqueous wash, etc.)?
Hi Rick,
No, it does not.
But yes, it is strongly recommended the port opening to be protected e.g. by adhesive Kapton tape or other means prior to the cleaning process to prevent contamination and foreign materials from being introduced into device as result of cleaning processes.
Best regards,
Tomas
Hi Tomas,
Thanks for the reply. Do you know if there are any plans in the future to provide the purchased part with a removable seal? The reason I am asking is because it is a small SMD device and there is risk and labor at the piece part level of unpackaging, handling, applying a seal and repackaging prior to loading on the placement machine for assembly.
Thanks,
Rick.