G-sensor FXLS8471Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

G-sensor FXLS8471Q

1,378 Views
monstor
Contributor II

I follow the AN4692 to configure my G-sensor. The output seems is normal. When we roll over the G-sensor, there is a normal output. However, after that the G-sensor output would become zero again immediately. We already disable the Auto-wake/sleep mode and low power mode. Please help.

Labels (1)
0 Kudos
2 Replies

1,009 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Henry,

It is hard to say where the problem might be. If you posted here your source code and ideally also timing diagrams from a logic analyzer, I might be able to help you in your investigation.

Meanwhile, you may find useful my simple FXLS8471Q bare-metal example code or another example code illustrating the use of the vector-magnitude function.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 Kudos

1,009 Views
monstor
Contributor II

Dear Tomas,

Below is my source code.

void Initial_GSensor(void)
{
     CS_B_PutVal(1);//int the CS to High 

      GSensor_Write_Addr_Cmd(XYZ_DATA_CFG, 0x12); // +/-8g range with ~0.976mg/LSB
//     Set_Roll_Over();
//     Set_Transient_Detection();  
       GSensor_Write_Addr_Cmd(CTRL_REG1, 0x39);    // ODR = 1.56Hz, Normal mode, Active mode
       GSensor_Write_Addr_Cmd(CTRL_REG2, 0x02);    // Reset, High Resolution mode
//     Get_GSensor_Calibration();
}


void Get_GSensor_XYZ(void)
{
   
    GSensor_Read_Addr_Cmd(OUT_X_MSB, 7);
    X_MSB = GSensor_Data[1];
    X_LSB = GSensor_Data[2];
    Y_MSB = GSensor_Data[3];
    Y_LSB = GSensor_Data[4];
    Z_MSB = GSensor_Data[5];
    Z_LSB = GSensor_Data[6];
   
    G_Sensor.Xout_14bit = ((X_MSB << 8) | (X_LSB))>>2; 
    G_Sensor.Yout_14bit = ((Y_MSB << 8) | (Y_LSB))>>2; 
    G_Sensor.Zout_14bit = ((Z_MSB << 8) | (Z_LSB))>>2;        
   
    if(G_Sensor.Xout_14bit >= TWO_COMPLEMENT){
      X = ((X_MSB << 8) | (X_LSB))>>2;                      //  flip all the 14 bits
      X = (X ^ 0x3FFF) + 1;     
      G_Sensor.Xout_g = X * SENSITIVITY * (-1);             // Compute X-axis output value in g's 
    }else{
      G_Sensor.Xout_g = G_Sensor.Xout_14bit*SENSITIVITY;    // Compute X-axis output value in g's     
    }   
   
    if(G_Sensor.Yout_14bit >= TWO_COMPLEMENT){
      Y = ((Y_MSB << 8) | (Y_LSB))>>2;                      //  flip all the 14 bits 
      Y = (Y ^ 0x3FFF) + 1;  
      G_Sensor.Yout_g = Y * SENSITIVITY * (-1);             // Compute Y-axis output value in g's 
    }else{
      G_Sensor.Yout_g = G_Sensor.Yout_14bit*SENSITIVITY;    // Compute Y-axis output value in g's     
    }
   
    if(G_Sensor.Zout_14bit >= TWO_COMPLEMENT){
      Z = ((Z_MSB << 8) | (Z_LSB))>>2;                      //  flip all the 14 bits
      Z = (Z ^ 0x3FFF) + 1;     
      G_Sensor.Zout_g = Z * SENSITIVITY * (-1);             // Compute Z-axis output value in g's     
    }else{
      G_Sensor.Zout_g = G_Sensor.Zout_14bit*SENSITIVITY;    // Compute Z-axis output value in g's     
    }
}

void Get_GSensor_Calibration(void)
{
  
    GSensor_Write_Addr_Cmd(CTRL_REG1, 0x18);   //Set device in 100 Hz ODR, Standby
   
    GSensor_Read_Addr_Cmd(OUT_X_MSB, 7);
    X_MSB = GSensor_Data[1];
    X_LSB = GSensor_Data[2];
    Y_MSB = GSensor_Data[3];
    Y_LSB = GSensor_Data[4];
    Z_MSB = GSensor_Data[5];
    Z_LSB = GSensor_Data[6];
   
    G_Sensor.Xout_14bit = ((X_MSB << 8) | (X_LSB))>>2; 
    G_Sensor.Yout_14bit = ((Y_MSB << 8) | (Y_LSB))>>2; 
    G_Sensor.Zout_14bit = ((Z_MSB << 8) | (Z_LSB))>>2;        
   
    X_offset = G_Sensor.Xout_14bit / 8 * (-1);
    Y_offset = G_Sensor.Yout_14bit / 8 * (-1);
    Z_offset = (G_Sensor.Zout_14bit - SENSITIVITY) / 8 * (-1);   
   
    GSensor_Write_Addr_Cmd(CTRL_REG1, 0x39);    // ODR = 1.56Hz, Reduced noise, Active mode
       

void GSensor_Read_Addr_Cmd(char Addr,word len)

  isoSPI1_TComData temp_char;   
  word i;

  Delay_ms_GSensor(1);

  CS_B_PutVal(0);//CS low
  
  Delay_ms_GSensor(1);
 
  Check_Value = 1;
  TimeOut_CNT = 0;
  while( (Check_Value != 0) && (TimeOut_CNT < 3000)){
    Check_Value = isoSPI1_SendChar( ((~0x80) & Addr) );   //  R/W, ADDR[6], ADDR[5], ADDR[4], ADDR[3], ADDR[2], ADDR[1], ADDR[0]
    TimeOut_CNT++;
  }   
 
  Check_Value = 1;
  TimeOut_CNT = 0;
  while( (Check_Value != 0) && (TimeOut_CNT < 3000)){
    Check_Value = isoSPI1_SendChar(Addr);                 //  ADDR[7], X, X, X, X, X, X, X
    TimeOut_CNT++;                               
  } 
 
  Delay_ms_GSensor(1);
 
  for(i=0;i<len;i++)
  {    
    isoSPI1_SendChar(0);                  //  dummy
   
    Check_Value = 1;
    TimeOut_CNT = 0;
    while( (Check_Value != 0) && (TimeOut_CNT < 3000)){
      Check_Value = isoSPI1_RecvChar(&temp_char);         //  DATA[7], DATA[6], DATA[5], DATA[4], DATA[3], DATA[2], DATA[1], DATA[0]
      TimeOut_CNT++;                               
    }   
    GSensor_Data[i] = temp_char;
  }
 
  Delay_ms_GSensor(1);
 
  CS_B_PutVal(1);//CS High
 
  Delay_ms_GSensor(1);
  
}

void GSensor_Write_Addr_Cmd(char Addr,char data)
{   

  Delay_ms_GSensor(1);

  CS_B_PutVal(0);//CS low
  
  Delay_ms_GSensor(1);
   
  Check_Value = 1;
  TimeOut_CNT = 0;
  while( (Check_Value != 0) && (TimeOut_CNT < 3000)){   
    Check_Value = isoSPI1_SendChar( ((0x80) | Addr) );   //  R/W, ADDR[6], ADDR[5], ADDR[4], ADDR[3], ADDR[2], ADDR[1], ADDR[0]
    TimeOut_CNT++;
  }
 
  Check_Value = 1;
  TimeOut_CNT = 0;
  while( (Check_Value != 0) && (TimeOut_CNT < 3000)){
    Check_Value = isoSPI1_SendChar(Addr);                //  ADDR[7], X, X, X, X, X, X, X
    TimeOut_CNT++;
  }
 
  Check_Value = 1;
  TimeOut_CNT = 0;
  while( (Check_Value != 0) && (TimeOut_CNT < 3000)){   
    Check_Value = isoSPI1_SendChar(data);                //  DATA[7], DATA[6], DATA[5], DATA[4], DATA[3], DATA[2], DATA[1], DATA[0]
    TimeOut_CNT++; 
  }
     
  Delay_ms_GSensor(1);
 
  CS_B_PutVal(1);//CS High

  Delay_ms_GSensor(1);
  
}

0 Kudos