FXLS8967AF - read FIFO?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXLS8967AF - read FIFO?

647 Views
andrewneil
Contributor III

I don't find the datasheet at all clear on how to read out the values from the FIFO.

Is it necessary to repeatedly read the individual triplets

 

for each triplet
{
   sensor_comm_read( handle, FXLS896xAF_BUF_X_LSB, 6, data );
}

 

 

Or will a single burst read get all the triplets

 

sensor_comm_read( handle, FXLS896xAF_BUF_X_LSB, number_of_triplets*6, data );

 

 

ie, does the auto-increment loop-back from BUF_Z_MSB to BUF_X_LSB so long as there is more data in the FIFO?

0 Kudos
7 Replies

631 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello andrewneil,

I hope all is great with you. Thank you for using the NXP communities.

The byte order of the output data is programmable via SENS_CONFIG2[LE_BE], and defaults to little-endian mode.

If SENS_CONFIG2[F_READ] = 1, the auto increment mechanism skips over the MSB registers. This operation shortens the output data size from 6 bytes to 3 bytes per XYZ sample.

I do recommend downloading the driver example from the link below and using it as a reference for your design.

Sensor Drivers for NXP Sensors

diazmarin09_0-1708020777152.png

 

I hope this information helps.

Regards,

David

0 Kudos

619 Views
andrewneil
Contributor III

I'm sorry, that doesn't answer the question at all.

The question is, to read the entire FIFO:

  1. can I read the entire FIFO with a single burst read, or
  2. must I do multiple burst reads - one for each (X,Y,Z) triplet ?

In other words, what happens in a burst read after reading BUF_Z_MSB (0x11):

  • does it "loop-back" to BUF_X_LSB (0x0C), or
  • does it carry on to PROD_REV (0x12) ?

I have downloaded the drivers - they do not illustrate this.

0 Kudos

588 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello andrewneil,

Please accept my apologies for the misunderstanding.

You are correct, should perform multiple burst reading procedures to read the entire buffer.  

Regards,

David

0 Kudos

549 Views
andrewneil
Contributor III

@diazmarin09 - should perform multiple burst reading procedures

Really?

As already noted, that Table 20 in the datasheet is very confusing:

https://community.nxp.com/t5/Sensors/FXLS8967AF-Confused-by-quot-Auto-increment-Address-quot/m-p/178...

But I think I've now managed to figure it out:

 

andrewneil_0-1708511825039.png

So a Normal (F_READ=0) burst read of 13 bytes starting at 0x0B should get:

  1. BUF_STATUS (0Bh)
  2. BUF_X_LSB  (0Ch)
  3. BUF_X_MSB  (0Dh)
  4. BUF_Y_LSB  (0Eh)
  5. BUF_Y_MSB  (0Fh)
  6. BUF_Z_LSB  (10h)
  7. BUF_Z_MSB  (11h)
  8. BUF_X_LSB  (0Ch)
  9. BUF_X_MSB  (0Dh)
  10. BUF_Y_LSB  (0Eh)
  11. BUF_Y_MSB  (0Fh)
  12. BUF_Z_LSB  (10h)
  13. BUF_Z_MSB  (11h)

Yes ?

Or have I still not understood Table 20 ?

 

0 Kudos

539 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello andrewneil,

I know that Table 20 is indeed confusing, but your understanding is correct. I mean, that is the expected registers sequence with the auto-increment feature and F_READ=0.

Regards,

David

0 Kudos

535 Views
andrewneil
Contributor III

Good.

So it should require just one burst to read the entire FIFO?

BUF_STATUS[BUF_CNT]  indicates the number of triplets required, so the total burst length required would be six times the BUF_STATUS[BUF_CNT] value ?

I know that Table 20 is indeed confusing

It certainly is!

I will update the other thread on that topic:

https://community.nxp.com/t5/Sensors/FXLS8967AF-Confused-by-quot-Auto-increment-Address-quot/m-p/178...

 

0 Kudos

524 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello andrewneil,

BUF_STATUS[BUF_CNT]  indicates the number of triplets required, so the total burst length required would be six times the BUF_STATUS[BUF_CNT] value?

You are correct, my apologies for the confusion. I do appreciate your efforts. 

Regards,

David