Hi, I am trying to implement code for the MC33771, but I'm struggling to make sense of the CRC description in the datasheet. It uses a 9 bit polynomial 0x12F, but on page 41 it shows, what I presume is, a hardware implementation where X8 is the same as X0, so X8 doesn't operate on the current CRC value, but on the incoming data from the stream. However, the diagram below it shows all 9 bits operating on the CRC.
I've been trying for several days to get this to work, using every combination I can think of, with no success. I have also tried a number of online checkers, all of which come up with different answers to the ones in the examples in the datasheet.
As this project has incredibly tight timescales, I'm really up against it, so if anyone has sample code that works with this polynomial or an algorithm that does, I would be very grateful.
Thanks
Andy
Hi Sir, i am writing code communicate with MC33771 through MC33664 ,using TPL Communication( sample code )
SPI0 as master (tx) - NXP S32K144
SPI2 as slave(rx)- NXP S32K144 -Microcontroller
i send write data via spi0 (TX),i am getting echo data only in spi2( rx)
NO RESPONSE FROM MC3371
it happen both write and read command
pls help me
Regards
Prabu.S
Hello Prabu,
I can provide you an example code as well as an application note with basic guidelines for the configuration and programming of the MC33771 BCC.
However, it cannot be shared without a signed NDA with your NXP Sales Representative or Distributor. Then please create a private support ticket.
Thank you for your understanding.
Best regards,
Tomas
Hello Andy,
What is the document number/URL of the manual you referred to? I can only find short factsheets (MC33664FS, MC33772FS, MC33772SM). I'm particularly interested as the CRC algorithm appears to be unique.
Thanks
Greg