Accelerometers: MMA845x vs FXLS8962

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Accelerometers: MMA845x vs FXLS8962

1,406 Views
atzelcollazo
NXP Employee
NXP Employee

Hello,

I'll be migrating my customer who is currently using the MMA8451QT and the MMA8452QR to the FXLS8962AF and I'd like to know if, at the SDK drivers level, they will have an easy migration process experience. I know both are different but I'm working if at the user level will be hard as well using the SDK drivers. 

 

Thanks,
Atzel Collazo

0 Kudos
3 Replies

1,366 Views
AmitPurohit
NXP Employee
NXP Employee

Hi @TomasVaverka and @atzelcollazo ,

FXLS8962AF is supported by ISSDK and available on MCUXpresso. FXLS8962AF sensor kit is FRDM-K22F-AGMP03 and user can generate/download this kit SDK from mcuxpresso.nxp.comSDK builder page.

Regards,

Amit Purohit.

0 Kudos

1,356 Views
atzelcollazo
NXP Employee
NXP Employee

Hello Amit,

How compatible are the user drivers from the MMA845x to the FXLS8962? If my customer is migrating from the MMA845x to FXLS8962, can they expect a smooth transition or will they need to start from scratch?

Regards,
Atzel Collazo

0 Kudos

1,389 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi @AmitPurohit,

 

Could you help with this request, please? Is the FXLS8962AF supported by ISSDK?

 

Best regards,

Tomas

0 Kudos