Known issue: STB GUI for eCompass kits returns error when using without Adobe Flash Player + ActiveX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Known issue: STB GUI for eCompass kits returns error when using without Adobe Flash Player + ActiveX

Known issue: STB GUI for eCompass kits returns error when using without Adobe Flash Player + ActiveX

Issue


Using the STB GUI for eCompass kits RD4247MAG3110 and RD4247FXOS8700 only -- v6.1.0.1 on a machine that does not have the Adobe Flash Player ActiveX program installed may run into the following error after pressing the eCompass button:


STB GUI error.JPG.jpg


Solution


Install the Adobe Flash Player + ActiveX from Adobe.



Let us know if you are facing any other issues with the STB GUI v6.1.0.1.


Regards,

Tomas


标签 (1)
无评分
版本历史
最后更新:
‎08-20-2014 07:20 AM
更新人: