FXLS8471 Breakout Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FXLS8471 Breakout Board

FXLS8471 Breakout Board

The FXLS8471Q Freescale accelerometer is highly versatile for industrial and consumer high-performance low-g applications that offer noise density, board mount offset, temperature performance and sensitivity. Integrated motion detection features include tilt, shake and tap detection with a new vector magnitude output that simplifies implementation and reduces power consumption. This new FXLS8471Q accelerometer has a SPI interface that is pin-compatible with Freescale’s industry-leading I2C accelerometer portfolio.


Here is a Render of the FXLS8471 Breakout- Board downloaded from OSH Park:

OSH_Render_TOP_BOT.png

And here is an image of the Layout Design for this board:

OSH_GTL.png

OSH_GBL.png


In the Attachments section, you can find the Schematic Source File (.SCH), Schematic PDF File, Layout Source File (BRD), Gerber Files (GTL, GBL, GTS, GBS, GTO, GBO, GKO, XLN) and BOM for this Breakout-board.

If you are interested in more designs like this breakout board for other sensors, please go to Freescale Sensors Breakout Boards Designs – HOME

附件
评论

Approved

Reyes

Can NXP provide the latest breakout board schematic and board files for the BRKOUT-FXLN8372Q? All the files above are older versions. They do not match the board which I received yesterdayIMG_5195.JPG.

无评分
版本历史
最后更新:
‎02-16-2015 02:34 PM
更新人: