sss_key_object_allocate_handle

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

sss_key_object_allocate_handle

跳至解决方案
448 次查看
A_Nawa
Contributor I

Hi Team,

I tried to run TLSClient example according to the following document.

/simw-top/doc/demos/linux/tls_client/tls_client_demo.html

But I got the next error message.Could you give me some advice on what to do to resolve this? 

 

My enviroment is 

 SE050:raspi3 + OM-SE050ARD-F
 OpenSSL: v3.0.12
 Plug and Trus Middleware V4.05.00

 

Error Message is

pi@raspberrypi:~/Project/nxp/se_mw/simw-top/demos/linux/tls_client/scripts $ python3 provisionTlsClient.py --key_type rsa
loading library from path: /home/pi/Project/nxp/se_mw/simw-top/tools/libsssapisw.so
SE050 Key provisioning script (Rev.0.9).
Executing this script will insert keys in the attached SE050 secure element.
###############################################################
#
# SUBSYSTEM : se05x
# CONNECTION_TYPE : t1oi2c
# CONNECTION_PARAMETER : none
#
###############################################################
sss :INFO :atr (Len=35)
00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08
01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41
54 50 4F
sss :WARN :Communication channel is Plain.
sss :WARN :!!!Not recommended for production use.!!!
sss_session_open SUCCESS
sss :WARN :nxEnsure:'ret == SM_OK' failed. At Line:7837 Function:sss_se05x_TXn
client_key file: /home/pi/Project/nxp/se_mw/simw-top/demos/linux/tls_client/scripts/../credentials/RSA/tls_client_key.pem
Injecting RSA key pair at key ID: 0x7dccbb30
sss_key_store_context_init SUCCESS
sss_key_store_allocate SUCCESS
sss_key_object_init SUCCESS
sss_key_object_init SUCCESS
sss :WARN :nxEnsure:'ret == SM_OK' failed. At Line:7837 Function:sss_se05x_TXn
sss :ERROR:Couldn't check if object id 0x7DCCBB30 exists
sss_key_object_allocate_handle FAILED
Traceback (most recent call last):
File "provisionTlsClient.py", line 365, in <module>
main()
File "provisionTlsClient.py", line 339, in main
status = set_rsa_pair(session, RSA_KEYPAIR_INDEX_CLIENT_PRIVATE, client_key)
File "provisionTlsClient.py", line 185, in set_rsa_pair
status = set_obj.do_set_rsa_key_pair(keyid, client_key, None)
File "/home/pi/Project/nxp/se_mw/simw-top/pycli/src/sss/setkey.py", line 278, in do_set_rsa_key_pair
key_type, cypher_type, policy)
File "/home/pi/Project/nxp/se_mw/simw-top/pycli/src/sss/setkey.py", line 442, in _set_key
self._key_object_mode)
File "/home/pi/Project/nxp/se_mw/simw-top/pycli/src/sss/keyobject.py", line 71, in allocate_handle
raise Exception("sss_key_object_allocate_handle %s" % status_to_str(status))
Exception: sss_key_object_allocate_handle FAILED

 

0 项奖励
1 解答
369 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @A_Nawa ,

 

Was OM-SE050ARD-F still used in this test? As far as I know, OM-SE050ARD-F doesn't support ECC crypto schemes except ECDSA.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
5 回复数
426 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @A_Nawa ,

 

I noticed you use OM-SE050ARD-F in the test, did you enable platformSCP03 in the authentication type when you build the MW? Please note for SE050F SCP03 is mandatory. Please kindly refer to https://www.nxp.com/docs/en/application-note/AN12436.pdf for details.

 

Please refer to chapter 5 in https://www.nxp.com.cn/docs/en/application-note/AN12570.pdf for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
418 次查看
A_Nawa
Contributor I

Hi Kan_Li, 

Thank you for you  support.

Yes, I use OM-SE050ARD-F with raspi3. I enabled platformSCP03 when I build the MW.

The se05_Minimal command exuecution was success.

pi@raspberrypi:~/Project/nxp/se_mw/simw-top_build/raspbian_native_se050_t1oi2c/bin $ ./se05x_Minimal
App :INFO :PlugAndTrust_v04.05.00_20231201
App :INFO :Running ./se05x_Minimal
App :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
App :INFO :Using default PlatfSCP03 keys. You can use keys from file using ENV=EX_SSS_BOOT_SCP03_PATH
sss :INFO :atr (Len=35)
00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08
01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41
54 50 4F
App :INFO :mem=29468
App :INFO :se05x_Minimal Example Success !!!...
App :INFO :ex_sss Finished

 

But I still got the next error when I run the provisionTlsClient.py.

sss :ERROR:Couldn't check if object id 0x7DCCBB30 exists
sss_key_object_allocate_handle FAILED

0 项奖励
402 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @A_Nawa ,

 

For python scripts , you have to specify the auth type as well as the platform scp keys. Please kindly refer to the following for details.

ubuntu@ubuntu:~/simw-top/demos/linux/tls_client/scripts$ python3 provisionTlsClient.py --key_type rsa --auth_type PlatformSCP --scpkey ~/simw-top_build/simw-top-eclipse_jrcpv1/bin/se050F_scp_keys.txt
loading library from path: /home/ubuntu/simw-top/tools/libsssapisw.so
SE050 Key provisioning script (Rev.0.9).
Executing this script will insert keys in the attached SE050 secure element.
###############################################################
#
# SUBSYSTEM : se05x
# CONNECTION_TYPE : t1oi2c
# CONNECTION_PARAMETER : none
#
###############################################################
sss_key_store_context_init SUCCESS
sss_key_store_allocate SUCCESS
sss :INFO :atr (Len=35)
00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08
01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41
54 50 4F
sss_session_open SUCCESS
client_key file: /home/ubuntu/simw-top/demos/linux/tls_client/scripts/../credentials/RSA/tls_client_key.pem
Injecting RSA key pair at key ID: 0x7dccbb30
sss_key_store_context_init SUCCESS
sss_key_store_allocate SUCCESS
sss_key_object_init SUCCESS
sss_key_object_init SUCCESS
sss_key_object_allocate_handle SUCCESS
sss_key_store_set_key SUCCESS
sss_key_store_save SUCCESS
Successfully Injected RSA key pair.
sss_key_store_context_init SUCCESS
sss_key_store_allocate SUCCESS
sss_key_object_init SUCCESS
sss_key_object_get_handle SUCCESS
sss_key_store_get_key SUCCESS
Successfully Created reference key.
certificate file: /home/ubuntu/simw-top/demos/linux/tls_client/scripts/../credentials/RSA/tls_client.cer
Injecting Certificate at key ID: 0x7dccbb31
sss_key_store_context_init SUCCESS
sss_key_store_allocate SUCCESS
sss_key_object_init SUCCESS
sss_key_object_init SUCCESS
sss_key_object_allocate_handle SUCCESS
sss_key_store_set_key SUCCESS
sss_key_store_save SUCCESS
Successfully Injected Certificate.
Closing port
##############################################################
# #
# Program Completed Successfully #
# #
##############################################################
ubuntu@ubuntu:~/simw-top/demos/linux/tls_client/scripts$

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
375 次查看
A_Nawa
Contributor I

Hi Kan_Li,

The provisionTlsClient.py executed successfully with --auth_type PlatformSCP.

Thank you for your support.

 

Next I try to run the ./tlsExtendedSeClient.sh. But I got the next error message,

Could you give me some advice on what to do?

 

pi@raspberrypi:~/Project/nxp/se_mw/simw-top/demos/linux/tls_client/scripts $ ./tlsExtendedSeClient.sh 192.168.121.15 EC
 
 
/home/pi/Project/nxp/se_mw/simw-top/demos/linux/tls_client/scripts
IOT_SE=se050
Config file is loaded in C example
Connecting to 192.168.121.15:8080
>> ../build/tlsSe050Client 192.168.121.15:8080 EC ../credentials/prime256v1/tls_rootca.cer nxp:0x7DCCBB10
../build/tlsSe050Client (Rev.0.9.2)
servername:port = 192.168.121.15:8080
keyType: EC
rootCA: ../credentials/prime256v1/tls_rootca.cer
clientKey: nxp:0x7DCCBB10
wrapConnectToSe: Open connection to secure element. 
App   :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
App   :INFO :Using default PlatfSCP03 keys. You can use keys from file using ENV=EX_SSS_BOOT_SCP03_PATH
sss   :INFO :atr (Len=35)
      00 A0 00 00    03 96 04 03    E8 00 FE 02    0B 03 E8 08 
      01 00 00 00    00 64 00 00    0A 4A 43 4F    50 34 20 41 
      54 50 4F 
sss   :WARN :nxEnsure:'ret == SM_OK' failed. At Line:7837 Function:sss_se05x_TXn
sss   :WARN :nxEnsure:'status == SM_OK' failed. At Line:4541 Function:sss_se05x_key_store_get_key
Fetching client certificate fails with status code: 0x3c3c0000.
Failed to retrieve client certificate.
 
******** TLS Client Example (Credentials in Secure Element) = Fail ********
"../build/tlsSe050Client 192.168.121.15:8080 EC ../credentials/prime256v1/tls_rootca.cer nxp:0x7DCCBB10" failed to run successfully, returned 1

 

0 项奖励
370 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @A_Nawa ,

 

Was OM-SE050ARD-F still used in this test? As far as I know, OM-SE050ARD-F doesn't support ECC crypto schemes except ECDSA.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励