How to port plug & Trust middle ware of SE050 with PN7462

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to port plug & Trust middle ware of SE050 with PN7462

1,240 Views
mohamedaslam_m
Contributor II

Hi folks ,

     I am pretty newbie with SE050, I want to create a SCP03 channel b/w PN7462 and SE050 over i2c. 

The options what I believe is to send APDU commands directly to the SE050 or port the Plug & Trust middle ware to  the PN7462 SDK and use the API to establish Secure channel protocol b/w the devices.

It will be greatly appreciated if any one can tell me how to port Plug & Trust middle ware with the PN7462 .

Thanks & Regards

Aslam

 

Labels (2)
0 Kudos
Reply
1 Reply

1,219 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @mohamedaslam_m ,

 

There is an app note regarding this topic, please refer to https://www.nxp.com/docs/en/application-note/AN12448.pdf for details.

 

There is also a similar use case available in https://community.nxp.com/t5/NFC-Knowledge-Base/Using-LPC55S69-with-SE050-and-CLRC663plus-for-Secure... , you may refer to it for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply