EEPROM device connecting via SPI interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EEPROM device connecting via SPI interface

1,940 次查看
Kazuma_Sasaki
Senior Contributor I

We would like to use the EEPROM device (P/N S25A080A) via SPI interface of S32V234.

Can S32V234 support device which using more than 32bits CMD?


Because, S25A080A is using 8, 16, 32 and more than 32bits CMD.

therefore, I worry about CMD FIFO can not support more than 32bits CMD.

Best Regards,

Kazuma Sasaki.

标记 (1)
0 项奖励
回复
1 回复

1,715 次查看
KushalShahNXP
NXP Employee
NXP Employee

Thanks for posting question. But we are now moving to ticketing system to support this device. This community will be closed soon.

So, I would encourage to raise a service request at www.nxp.com/support using "Support Requests" option and experts will help you with your questions.

 

-Kushal

0 项奖励
回复