tresos Studio 23.0 Activation problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

tresos Studio 23.0 Activation problem

5,382 次查看
ywjack
Contributor III

I downloaded the tresos Studio 23.0 software on the NXP official website. The official website provides an activation code that shows that it can be used until March 30, 2021. However, when I activate, it always prompts that the server cannot be connected. I don't know what caused this. I am using S32K144 MCU

Err:

INFO: Trusted Storage initialization done.
Manual Node-Locked License Activation processing ...
ERROR: Processing response (50019,41200,10246)
Activating NodeLocked License XXXX-XXXX-2960-3980, Number Of Licenses: 1
Status: 4, Creating request

Status: 5, Request created

Status: 6, Context created

Status: 0, Error

ERROR: flxActAppActivationSend (50041,41143,34)
Connection to FlexNet Operations Server failed.
Activating NodeLocked License XXXX-XXXX-2960-3980, Number Of Licenses: 1
Status: 4, Creating request

Status: 5, Request created

Status: 6, Context created

Status: 0, Error

ERROR: flxActAppActivationSend (50041,41143,34)
Connection to FlexNet Operations Server failed.
Activating NodeLocked License XXXX-XXXX-2960-3980, Number Of Licenses: 1
Status: 4, Creating request

Status: 5, Request created

Status: 6, Context created

Status: 0, Error

ERROR: flxActAppActivationSend (50041,41143,34)
Connection to FlexNet Operations Server failed.

0 项奖励
回复
6 回复数

5,349 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello,

Another way is you can try with Offline activation. Click to "Create Activation Request", then save the activation request file. Access to https://www.elektrobit.com/support/licensing/ then follow the instruction.

Regards,

Nam

0 项奖励
回复

5,338 次查看
ywjack
Contributor III

I will try what you said, thank you very much

0 项奖励
回复

5,361 次查看
hungnguyenphi
NXP Employee
NXP Employee

Dear ywjack,

From the error message, we can see that "Connection to FlexNet Operations Server failed". Then could you please check your internet connection. I still can use the your activation code normally. 

Could you please also share the "Elektrobit Client License Administration" 's version which you are using.

Best regards,

Hung.

 

0 项奖励
回复

5,358 次查看
ywjack
Contributor III

Hi :hungnguyenphi

The version I use is 1.2.4, I also try to use other versions to activate the phenomenon is the same as shown below

Thank you微信截图_20210104143754.png

0 项奖励
回复

4,628 次查看
yangyuze
Contributor I

Is your problem solved? I also encountered the same problem, how can I activate it successfully?

0 项奖励
回复

5,352 次查看
hungnguyenphi
NXP Employee
NXP Employee

Hello ywjack,

I also try to check the activation code with the version 1.2.4 and it still work. Then I am pretty sure that you have some issue with the internet connection. Could you please help to check with your company 's IT.

EB.png

Best regards,

Hung

0 项奖励
回复