simulation for pitch shifting at I2S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

simulation for pitch shifting at I2S

881 Views
erdoganguler
Contributor II

Hello,

 I am new on I2S protocol. I have a question. 

I have s32k148 board and fda903d amplifier. I have a sound data ( voice record)  in flash. I am reading that sound and writing in buffer in RAM ( ring buffer ).

I have also adc to change pitch ( not actual pitch).

for example  audio data in buffer seems like  ( sx : 32bit sample): 

s1,s2,s3,s4,s5,s6....s512

if ı want to increase frequency , I want to send data to I2S like ( jumping samples )

s1,s2,s3,s4,s5,s7 

or

s1,s2,s4,s5,s7,s9

and if ı want to decrease frequency  , I want to send data to I2S like ( repeat samples)

s1,s2,s2,s3,s4,s5,s5,s6,s7

or for more slow

s1,s2,s2,s3,s3,s4,s5

Now , at processor expert there is a function to send data to i2s, that function needs I2S instance, buffer pointer and sample count. but it plays like that: 

s1,s2,s3,s4,s5,s6,s7.

Q1: how can i jump or repeat samples ?

Q2: is it possible to send samples by one by without changing sample rate of sound ? should ı use timer for that ? or is there a periodic interrupt for every sample time in SAI

Tags (3)
0 Kudos
Reply
2 Replies

823 Views
Learner
Contributor III

@erdoganguler @Alexis_A  I am new with S32K and SAI. I am trying to use SAI to interface fda903d amplifier with S32K148 but getting alot of issues. If you can share some reference code it would be a great help for me. Thanks

0 Kudos
Reply

830 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Erdogan,

Q1: How can I jump or repeat samples?

For this, the best way would be to set the buffer with the samples you want. In the API, there isn't any way to skip examples.

Q2: is it possible to send samples by one by without changing the sample rate of sound ? should ı use timer for that ? or is there a periodic interrupt for every sample time in SAI

Yes, it is possible but if you do this I don't think the sound quality will be the best, you only need to take care of the fetching to the I2S bus so there aren't any gaps in the audio transmission. Also, the callback could be used to control the fetching.

Let me know if this helps you.

Best Regards,

Alexis Andalon

0 Kudos
Reply