Hi NXP,
i want test secure debug on S32K312,and hope not to advanced to OEM_PROD before finish whole development.
i am now in CUST_DEL and ADKP programed.
i see some doc metioned "Simulated_OEM_PROD" but it's not described in detail. my question is:
1. is it now available in HSE 2.40.0?
2. precondition to set it? currently i only set ADKP(raw mode) and use hse service to set, but failed with aa55a21c.
3. if set it done, is it sufficient to test secure debug?
4. in Simulated_OEM_PROD, after chip reset, what's LC now? is it can fully back to CUST_DEL?
Hi @victory
1. is it now available in HSE 2.40.0? Yes.
2. precondition to set it? currently i only set ADKP(raw mode) and use hse service to set, but failed with aa55a21c. You can find more information in the HSE Service API Reference Manual.
3. if set it done, is it sufficient to test secure debug? Could you specify what you are looking to test?
4. in Simulated_OEM_PROD, after chip reset, what's LC now? is it can fully back to CUST_DEL? Yes, after a reset the MCU returns to CUST_DEL.
BR, VaneB