Hello,
I'm having a problem with s32k312 where the mcu keeps resetting while the code is running.
I have encountered a problem similar to this one.
Solved: Re: Query about Reset problem in S32K344 - NXP Community
I saw a similar issue saying it was a Core clock or Hse clock configuration issue, but I checked and found that it did not (CoreClock=120M, HseClock=120M),
and I also noticed this
I would like to ask
1.if there is a boundary error (i.e. at CoreClock=120M, HseClock cannot be equal to 120M, it can only be 60M)
2.if there are other issues that cause this phenomenon
Thank you.
No such error is known to me.
It is needed to keep one of mentioned clocking option.
Do you specifically see HSE as reset reason as mentioned in the highlighted thread?