s32k144 implement PIC with IAR.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k144 implement PIC with IAR.

970 Views
StephenYeh
Contributor III

Our project needs to be compiled into PIC (Position Independent Code) function with IAR.


1. The following is the error message generated by using the IAR compile tool. 

S32DS_IAR_Converter.out
Error[Lp005]: placement includes a mix of sections with content (example "ro data preinit_array section .prepreinit_array in clockMan1.o") [suitable for placement in ROM] and sections without content (example "rw data section .data in clock_S32K1xx.o") [suitable for placement in RAM] D:\workspace_S32DS_for_IAR\IAR_S32DS\Project_Settings\Linker_Files\S32K144_64_flash.icf 152
Error[Lt043]: Base relative relocation to non-static base address.
Relocation: R_ARM_SBREL32
Destination: "g_pin_mux_InitConfigArr"
Location: "CCIF_Handler" + 0x14
Error[Lt043]: Base relative relocation to non-static base address.
Relocation: R_ARM_SBREL32
Destination: "CLOCK_SYS_GetDefaultConfiguration::peripheralClockConfig"
Location: "CLOCK_DRV_GetFreq" + 0x5f0
Error[Lt043]: Base relative relocation to non-static base address.
Relocation: R_ARM_SBREL32
Destination: "clockMan1_InitConfig0"
Location: ".text14" + 0x14
Error[Lt043]: Base relative relocation to non-static base address.
Relocation: R_ARM_SBREL32
Destination: "peripheralClockConfig0"
Location: "??__sti__routine_0" + 0x4
Error[Lt043]: Base relative relocation to non-static base address.
Relocation: R_ARM_SBREL32
Destination: "xFreeBytesRemaining"
Location: "vPortFree" + 0x7c
Error[Lt043]: Base relative relocation to non-static base address.
Relocation: R_ARM_SBREL32
Destination: "g_lpspiBase"
Location: "LPSPI_DRV_MasterIRQHandler" + 0xc8
Error[Lt043]: Base relative relocation to non-static base address.
Relocation: R_ARM_SBREL32
Destination: "g_lpspiBase"
Location: "LPSPI_DRV_DisableTEIEInterrupts" + 0x30
Error[Lt043]: Base relative relocation to non-static base address.
Relocation: R_ARM_SBREL32
Destination: "g_lpspiBase"
Location: "LPSPI_DRV_SlaveAbortTransfer" + 0x76
Error[Lt043]: Base relative relocation to non-static base address.
Relocation: R_ARM_SBREL32
Destination: "uxCriticalNesting"
Location: "vPortValidateInterruptPriority" + 0x58
Error[Lt041]: Absolute relocation to movable block.
Relocation: R_ARM_ABS32
Destination: "SystemInit" (in movable block: ROPI)
Location: "Reset_Handler" + 0x34 (in movable block: ROPI)
Error[Lt041]: Absolute relocation to movable block.
Relocation: R_ARM_ABS32
Destination: "init_data_bss" (in movable block: ROPI)
Location: "Reset_Handler" + 0x38 (in movable block: ROPI)
Error[Lt041]: Absolute relocation to movable block.
Relocation: R_ARM_ABS32
Destination: "pxCurrentTCB" (in movable block: RWPI)
Location: "vPortEnableVFP" + 0x10 (in movable block: ROPI)

Total number of errors: 13
Total number of warnings: 0

Build failed

See what's the problem?

2. Are there any other suggestions on the function of generating PIC?

0 Kudos
2 Replies

820 Views
StephenYeh
Contributor III

Hi Varun

Sorry, it didn't fixed.

0 Kudos

829 Views
varun_S22
Contributor I

how did you fix this error?

0 Kudos