s32k118 sleep mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k118 sleep mode

Jump to solution
1,668 Views
종찬박
Contributor II

Hi,

I'm Jongchan.

Let me ask you question about sleep mode for S32k118.

First, I need to output in sleep mode.

For example, Before sleep mode, the board turn on LED. and then After Sleep mode, it have to remain LED on.

so, Do I have to select only VLPR mode to implement above case? Isn't there any thing else?

(in datasheet, VLPR mode consumes more 1 mA. I have to satisfy lower current under 0.5mA)

Second, How do I configurate to wake up via CAN communication?

I refer to AN5425(Power Management for S32K1xx). but there is not How to configurate wake-up source.

I want you to get me the code like AN5425 example source.

Third, What is the function "scg_disable_pll_and_firc()"?

could you show me the code of function "scg_disable_pll_and_firc()" that is in 5.5.2 of the AN5425?

 

Thanks,

BR,

Jongchan

0 Kudos
1 Solution
1,605 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for the late reply!
I can not find the function "scg_disable_pll_and_firc()" code either.
Please refer to the similar function code in the SDK
POWER_DRV_DisableVlpClockSrc

POWER_DRV_DisableVlpClockSrc.png

View solution in original post

0 Kudos
3 Replies
1,659 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Jongchan,

Input / Output (I/O) states are maintained during all power modes.

Input Output (I O) states are maintained during all power modes.png

About how to wake up via CAN communication, you can refer below articles:
Example S32K116 FlexCAN PN STOP S32DS.ARM.2.2
Example S32K116 FlexCAN VLPR test S32DS.ARM.2.2
S32K1xx SDK FlexCAN sample projects to demonstrate its basic and advanced features

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,644 Views
종찬박
Contributor II

Hi Robin,

thanks for your response.

 

I'm developing my application with using low level peripheral driver even CAN Communication.

So, I need the function "scg_disable_pll_and_firc()" code. then, I would be able to clear my problem.

could you send me?

 

And, considering the consumption current, I have to use the VLPS mode.

But the example you sent is the project usint the SDK. so I couldn't use your example.

could you send me the low level code using VLPS via CAN wake up?

 

Best Regards,

Jongchan.

 

0 Kudos
1,606 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for the late reply!
I can not find the function "scg_disable_pll_and_firc()" code either.
Please refer to the similar function code in the SDK
POWER_DRV_DisableVlpClockSrc

POWER_DRV_DisableVlpClockSrc.png

0 Kudos