s32k bist

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k bist

3,583件の閲覧回数
Higgs_Boson
Contributor I

Hi, 

We are now evaluate the S32K BIST feature, when the sw call the api  Bist_Run() to initiated the bist , but the mcu reset. It happened in 

Bist_SelfTestTrigger() 

SAFETYBASE_REG_WRITE32(BIST_MC_RGM_ERCTRL_REG, BIST_MC_RGM_EASSERT_MASK);
 
Please anyone could help to resolve this issue?
0 件の賞賛
返信
12 返答(返信)

3,548件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Could you check the registers status right after the MCU is reset after executing Bist_Run(). The status should be as following:

namnguyenviet_0-1668670671138.png

namnguyenviet_1-1668670719073.png

Best Regards,

Nam

0 件の賞賛
返信

3,189件の閲覧回数
Higgs_Boson
Contributor I

Thanks That support.

 A new problem occur. When Enable the Bist Feature , the MCU gose into HardfaultHandler when use Trace32 in debug. But It is Normal without trace32 in debug. 

Please help to solve this issue. Thanks.

PS: BIST is Done without Trace32 debug. 

Higgs_Boson_0-1678691583997.png

 

 

0 件の賞賛
返信

3,111件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Since this ticket is quite long time ago and hence difficult to track, can you create another one?

Thank you.

Nam

0 件の賞賛
返信

3,538件の閲覧回数
Higgs_Boson
Contributor I

 the registers status right after the MCU is reset after executing Bist_Run().

Higgs_Boson_0-1668784526246.png

Higgs_Boson_1-1668784563413.png

 

And the attach file shows the registers list  with bist run after power on reset, before Bist_SelfTestTrigger()is call.

Higgs_Boson_2-1668784652926.png

 

Please help to analyse it , Thanks. 

 

0 件の賞賛
返信

3,517件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Not sure why the issue has occurred. Did you verify our demo code?

Best Regards,

Nam

0 件の賞賛
返信

3,558件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please try to go over the Bist_Run() function. After that, eventually a reset will be occurred according to the BIST sequence mentioned in RM

namnguyenviet_0-1668582981018.png

After reset, you can verify the status of the BIST in SCTU registers.

Best Regards,

Nam

0 件の賞賛
返信

3,557件の閲覧回数
Higgs_Boson
Contributor I

hi,

Thanks the reply.

The bist status is clear after reset , so i think it is not a functional reset. 

following screenshot is attach to s32k after it reset :

 

Higgs_Boson_0-1668586188192.png

 

0 件の賞賛
返信

3,425件の閲覧回数
Mohamed_abdelrazek
Contributor I

I need to find example project for BIST on S32K controller, can anyone help me ?

 

0 件の賞賛
返信

3,421件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Which package are you referring to?

Best Regards,

Nam

0 件の賞賛
返信

3,410件の閲覧回数
Mohamed_abdelrazek
Contributor I

Hello,
S32K344

0 件の賞賛
返信

3,400件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please download S32K3 Safety Peripheral Drivers version 1.0.1 from https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-general-pu... - S32K3 Standard Software:

namnguyenviet_1-1673334681000.png

After that, install the following package, and make sure that you have selected "S32K3 SPD Demo application"

namnguyenviet_0-1673334545253.png

Best Regards,

Nam

 

0 件の賞賛
返信

2,903件の閲覧回数
Sheon
Contributor I

Is there any example code for SAF BIST (S32K344)

0 件の賞賛
返信