s32k 1443vk board multiple channel frequency measurment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32k 1443vk board multiple channel frequency measurment

351 次查看
sandeepc
Contributor III

hi commuity i need to measure the frequency of ptd0,pte11, ptd1 before iam trying to configure all channel iam configuring for one channel but i configured input where it must call the call back funtion it hasnt calling any call back funtion i gone ic_pal example int that example its not going to the call back funtion 

so where can i find the example for configuring the callback function in s32k?

@S32K_tj 

0 项奖励
2 回复数

286 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

This question is the same as the s32k input frequency measurement, please do not submit the question repeatedly. I will answer you there.


Best Regards,
Robin

0 项奖励

261 次查看
sandeepc
Contributor III
sure iam checking with that
0 项奖励