Hello,
I am a developer developing with S32K148.
I ended up using the S32K148 on a new project.
I have installed S32 Design Studio for ARM Version 2.2.
And, I tried to run the S32K148_Project_Hello sample code.
However, an error message occurred as shown in the picture below.
I think the part I set is wrong.
But I don't know what the problem is.
I set it up as pictured below.
Please point out the problem to me.
thanks,
Hello @s_kim1,
If you use PE Micro Multilink, you need to use the GDB PEMicro interface.
Please go to Help / Install New Software
Select PE Micro Update side and install the interface
Regards,
Daniel
I completed the installation, but the problem still occurs.
Please see the picture below.
First, right-click the project and run it as Debug As->S32DS C/C++ Application.
An error has occurred.
Second, I run Debug As->Debug Configurations..
And add Executable: ${cross_prefix}gdb${cross_suffix} and run
It runs fine.
After that, if I try the first method(right-click the project and run it as Debug As->S32DS C/C++ Application.), the same error occurs.
I'm repeating this behavior every time I run it.
It's too inconvenient.
If you additionally run As, an error occurs as shown in the picture below.
Please tell me how to run it as Debug As->S32DS C/C++ Application.
I used CodeWarrior for MCU Version: 11.1 in the past.
CodeWarrior for MCU Version: 11.1 was easy and comfortable to use.
However, the currently used S32 Design Studio for ARM Version: 2.2 is too inconvenient.
please help me.
thanks,