<S32K1xx系列MCU应用指南之FlexIO模块使用详解>的样例工程

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

<S32K1xx系列MCU应用指南之FlexIO模块使用详解>的样例工程

Jump to solution
379 Views
lzx
Contributor II

<S32K1xx系列MCU应用指南之FlexIO模块使用详解>详细介绍了S32K144芯片上FlexIO模块的使用。其中使用的样例工程在哪里可以下载?特别是`S32K1xx_SDK_RTM3_0_SPIFlash_lpSPI_DMA_FlexIO_i2s`这个样例工程。

0 Kudos
Reply
1 Solution
292 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @lzx,

Are you using Enwei Hu's post from S32K1xx系列MCU应用指南之FlexIO和CSEc硬件加密模块的使用详解 (qq.com)?

If so, all the resources are posted on the article (download link is at the bottom), please contact the creator instead as this is not NXP official software and we are unable to provide support.

Best regards,
Julián

View solution in original post

0 Kudos
Reply
4 Replies
355 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @lzx,

Are you referring to AN12174? You can find the associated SW under the application note in "Documentation" from the S32K1 General-Purpose MCUs' page:

Julin_AragnM_0-1712857419363.png

Julin_AragnM_2-1712857430598.png

Best regards,
Julián

0 Kudos
Reply
343 Views
lzx
Contributor II

Thanks for your kind reply. But they're different demo. I need the demo which containing SPI+DMA+FlexIO i2s. 

mmexport9ecff37650f7bda2b230f4631c77da82_1712895458747.png

0 Kudos
Reply
293 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @lzx,

Are you using Enwei Hu's post from S32K1xx系列MCU应用指南之FlexIO和CSEc硬件加密模块的使用详解 (qq.com)?

If so, all the resources are posted on the article (download link is at the bottom), please contact the creator instead as this is not NXP official software and we are unable to provide support.

Best regards,
Julián

0 Kudos
Reply
288 Views
lzx
Contributor II

@Julián_AragónM Hi., 

that's correct. i contacted the author of the article and got the resources i wanted. Thanks a lot!