linstack bug after master sends multiframe (DS3.4, SDK RTM 4.0.3)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linstack bug after master sends multiframe (DS3.4, SDK RTM 4.0.3)

225件の閲覧回数
cf_st
Contributor I

Hi all, I am developing a lin application using S32k118 micro-controller, s23DS 3.4 and SDK RTM 4.0.3.

I think I found a bug in linstack library, I don't know if this is the most suitable place for signaling it. 

I am experiencing a vector catch issue when I try to send a multiframe master request (e.g. UDS service $2E, total payload 11 bytes) and then I try to perform a send even a single frame command (e.g. UDS service $22, total payloads 3 bytes).

From debugging it seems that in the function tl_receive_message() (in lin_commontl_proto.c file), the assignation of the length within the switch(PCI_type), for how it is implemented, causes it the length variable tmp_length to wrap around in case of first a longer message (e.g. multiframe) and then a shorter one. In the end, this leads to an attempt to write the buffer at an index greater then buffer dimension, thus vector catch.    

I implemented a fix that seems to resolve the issue, (snapshot below), can anyone tell me if this is a known issue? Is solved in a different SDK version for DS 3.4 (so RTM > 4.0.3)? Furhtermore, may the posted fix have potential problematic drawbacks? 

Thank you in advance and BR

 static void tl_receive_message(l_ifc_handle iii)

{

     ...

/* Single frame */
case PCI_SF:

  tmp_length = (l_u16)((l_u16)pdu[1] & 0x000FU); 

/* Swapped assignation of variables */

//              i = *length;
//              *length = tmp_length;
                *length = tmp_length;
                i = *length;
 
/* Commented if branch */
//                if (i < tmp_length)
//                {
//                   tmp_length = i;
//                }

 

....

          /* Multi frame */
            case PCI_FF:
                /* First frame */
               tmp_length = (l_u16)((((l_u16)pdu[1] & 0x000FU) << + (l_u16)pdu[2]);
               /* Swapped assignation of variables */
//                i = *length;
//                *length = tmp_length;
                *length = tmp_length;
                i = *length;
 
/* Commented if branch */
//                if (i < tmp_length)
//                {
//                    tmp_length = i;
//                }
 
       
               
0 件の賞賛
返信
1 返信

146件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

asked SW team, but got not feedback yet.

BR, Petr

0 件の賞賛
返信