how to upgrade module configurations to new module versions in EB Treasos

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to upgrade module configurations to new module versions in EB Treasos

1,006 次查看
wanghanlin
Contributor I

I installed two vesion MCAL.

My peoject base on old version.

I want upgrade module configurations to new module versions.

But there is no new version in upgrade window.

wanghanlin_3-1651641929305.png

 

The installation steps are as follows:

wanghanlin_0-1651641853943.png

 

wanghanlin_1-1651641876546.png

wanghanlin_2-1651641902102.png

 

 

 

标记 (1)
0 项奖励
2 回复数

987 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello,

You're right. Unfortunately, due to that derivate change, you need to create a new project based no RTM 1.0.5, then import the configuration from RTM 1.0.0 to that new project.

Best Regards,

Nam

0 项奖励

1,001 次查看
wanghanlin
Contributor I

I found that the derivate of the two versions do not match.This is why it can't be updated.

 

wanghanlin_0-1651650351096.png

 

0 项奖励