Hello,
Recently I was working on a project using the S32K344 chip, and while using flash I found a problem that the area between 0x0040 0000 and 0x0050 0000 could not be erased. However, erasing after 0x0050 0000 is no problem.
解決済! 解決策の投稿を見る。
Hi @Jackson_Ping,
The memory in the range of 0x400000 - 0x500000 is Block 0.
S32K3xx_Memory_Map.xlsx
While the flash controller is performing a flash operation at Block 0, the cores and other masters must not access the block.
Refer to AN13388 S32K3 Memories Guide
Here is a discussion on how to place the C40_Ip driver into SRAM:
https://community.nxp.com/t5/S32K/S32K344-C40-IP-Hardware-Fault-Problem/m-p/1697432
Regadrs,
Daniel
Hi @Jackson_Ping,
The memory in the range of 0x400000 - 0x500000 is Block 0.
S32K3xx_Memory_Map.xlsx
While the flash controller is performing a flash operation at Block 0, the cores and other masters must not access the block.
Refer to AN13388 S32K3 Memories Guide
Here is a discussion on how to place the C40_Ip driver into SRAM:
https://community.nxp.com/t5/S32K/S32K344-C40-IP-Hardware-Fault-Problem/m-p/1697432
Regadrs,
Daniel
Hi,@danielmartynek
I have understood.
Thank you very much for your answer!
Best Regards,
Jackson