entry to High-Speed Run (HSRUN) mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

entry to High-Speed Run (HSRUN) mode

跳至解决方案
208 次查看
xx1
Contributor I

Hi,

I am learning how to use the S32K144 board using the S32K-RM.

I want to enter to High-Speed RUN mode (HSRUN), and I found the method in S32K-RM as below. 

It seems there are two ways and I want to ask why in the first way we have to disable SPLL but in the next way we don't need to.

I hope to get your help.

Thank you!

xx1_0-1713346219542.png

 

 

0 项奖励
回复
1 解答
188 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @xx1,

In the first method, you are changing the clock for RUN and HSRUN, and reconfiguring PLL back. The reference manual states: "Selecting a different clock source when in RUN requires that clock source to be enabled first and be valid before system clocks switch to that clock source."

In the second method, SPLL is configured at 80MHz in RUN mode and use this clock source in HSRUN, no changes to the clock are needed.

You can look into the following document for additional information: AN5425: Power Management for S32K1xx

Best regards,
Julián

在原帖中查看解决方案

0 项奖励
回复
1 回复
189 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @xx1,

In the first method, you are changing the clock for RUN and HSRUN, and reconfiguring PLL back. The reference manual states: "Selecting a different clock source when in RUN requires that clock source to be enabled first and be valid before system clocks switch to that clock source."

In the second method, SPLL is configured at 80MHz in RUN mode and use this clock source in HSRUN, no changes to the clock are needed.

You can look into the following document for additional information: AN5425: Power Management for S32K1xx

Best regards,
Julián

0 项奖励
回复