i have a question, don't used to CANFD with this model(FS32K148UJVLQ) ,when i try to init CANFD, it will brake program and stop here,if i set it as normal CAN ,run is ok,not error. and i donot find this model in your official website,i don't know that this model is not support CANFD.
yes,i bought it from an official distributor
Hi,
CAN FD is functional on this device. Not sure what code/driver do you use and how module is configured. Note it operates using the non-ISO CAN FD protocol upon reset, so be sure other nodes on bus are configured for the same and set CTRL2[ISOCANFDEN] bit accordingly.
Obviously ISO CAN FD protocol is required and so CTRL2[ISOCANFDEN] should be set
BTW, I have received a confirmation that part number is OK.
Best regards,
Ladislav
Hi,
The table bellow corresponds to a data sheet data.
You should have some of these ...considering VLQ part....
FS32K148UJT0VLQR
FS32K148UJT0VLQT
Have you bought it from an official distributor?
Best regards,
Ladislav