can you provide address and description of memory swap registers for S32k344 and code example, please?
what configuration of S32 development studio and libraries etc. should be installed to run bootloader?
Hi
If you have access to Secure Files, please download AN744511 Secure Boot Application note v0.1.1.0 and SW745310 SecureBootAppNoteDemo.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
do you have code example to download?
provided example cannot be compiled on S32 Design studio v3.5 due incompatible drivers version RTD4.7 vs RTD4.4. do you have adjusted example for S32 Design studio v3.5?
Sorry, no example based on the new version of RTD were found.
Please download the code example(SW745310 SecureBootAppNoteDemo) from Secure Files
what configuration, version of S32 development studio and libraries and version etc. should be installed to run bootloader?
This document and related demo projects are valid for HSE-FW(FULL_MEM and AB_SWAP) version 0.1.1.0 and RTD version 1.0.0 only. You may need to install S32DS v3.4.1.
1. can you provide link to S32 studio ,SDK, library, please?
2. can I have simultaneously two S32 studio versions installed on my computer?
Please start from page 17 of S32K3xx Real-Time Drivers (RTD) Installation Guide - Training
Click S32K3 Standard Software - > Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M -> Previous -> S32K3 Real Time Drivers Version 1.0.0
Click S32K3 Standard Software - > Automotive SW - S32K3 - S32 Design Studio -> 3.4.1_D2110 S32 Design Studio for S32 Platform v.3.4 Update with Service Pack 2 for S32K3 devices