about S32KSDK lin_master_baremetal_s32k148

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about S32KSDK lin_master_baremetal_s32k148

3,460 Views
15736231627
Contributor II

When lin is used as the Master and the LIN host scheduling table has multiple ID, when receiving and sending are processed at the same time in the LIN interrupt, ID data loss and garbled code will occur.The following is my source code, please take a look at it for me,thanks

this is lin callback function:

 lin_callback_t lin_rx_tx_handle_callback(uint32_t instance, lin_state_t * lin1_State)
{
lin_callback_t callbackCurrent;
callbackCurrent = lin1_State->Callback;
uint8_t lin_id_index = 0;//lin number index

switch (lin1_State->currentEventId)
{
case LIN_PID_OK:
/* Set timeout */
LIN_DRV_SetTimeoutCounter(INST_LIN1, TIMEOUT);

for(lin_id_index = 0; lin_id_index < MASTER_FRAME_COUNT; lin_id_index++)
{
if(g_lin_master_schedule_list_config[lin_id_index].ID == lin1_State->currentId)
{ /* If PID is FRAME_TX_RSP, salve node will receive data from master node */
if(g_lin_master_schedule_list_config[lin_id_index].Type == FRAME_TX_RSP)
{
/* Call to Send Frame DATA Function */
LIN_DRV_SendFrameData(INST_LIN1, g_lin_master_Pdu_Matrix[lin_id_index].buf, sizeof(g_lin_master_Pdu_Matrix[lin_id_index].buf));
break;
}
else if(g_lin_master_schedule_list_config[lin_id_index].Type == FRAME_RX_RSP )
{
/* Call to Receive Frame DATA Function */
//current_id_sn = lin_id_index;
//receive_new_frame_flag = 1;
LIN_DRV_ReceiveFrameData(INST_LIN1, g_lin_master_Pdu_Matrix[lin_id_index].buf, sizeof( g_lin_master_Pdu_Matrix[lin_id_index].buf));
break;
}

else
{

}
}
}
break;
/* If PID is FRAME_GO_TO_SLEEP, salve node will go to sleep mode */

case LIN_PID_ERROR:
/* Go to idle mode */
LIN_DRV_GoToSleepMode(INST_LIN1);
break;
case LIN_TX_COMPLETED:

case LIN_RX_COMPLETED:
/* Go to idle mode */
LIN_DRV_GotoIdleState(INST_LIN1);
break;
case LIN_CHECKSUM_ERROR:
case LIN_READBACK_ERROR:
case LIN_FRAME_ERROR:
case LIN_RECV_BREAK_FIELD_OK:
/* Set timeout */
LIN_DRV_SetTimeoutCounter(INST_LIN1, TIMEOUT);
break;
case LIN_WAKEUP_SIGNAL:
/* Set wakeup signal flag */
// wakeupSignalFlag = true;
break;
case LIN_SYNC_ERROR:
case LIN_BAUDRATE_ADJUSTED:
case LIN_NO_EVENT:
case LIN_SYNC_OK:
default:
/* do nothing */
break;
}
return callbackCurrent;
}

Labels (1)
Tags (1)
0 Kudos
Reply
10 Replies

3,290 Views
15736231627
Contributor II

How to increase the frame slot and frame duration, or how to optimize my program?

0 Kudos
Reply

3,290 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try

#define TIME_BASE  5

const struct_lin_master_config g_lin_master_schedule_list_config[5] =
{
{0x14,8,FRAME_TX_RSP,2},
{0x21,8,FRAME_TX_RSP,6},
{0x3A,8,FRAME_RX_RSP,10},
{0x0C,8,FRAME_RX_RSP,14},
{0x02,8,FRAME_RX_RSP,18},
};

I cannot test the project. It gives me some PE errors.

BR, Petr

0 Kudos
Reply

3,290 Views
15736231627
Contributor II

I looked for a problem later. The reason why there is a frame error in my code is that the LIN configuration table I configured is inconsistent with the actual received byte length, and another reason is that the frame gap is set too small, but now I have extended the frame gap to 50ms to send a frame request, but occasionally there are a few error frames, but I have no problem with the frame gap 10ms on other MCU platforms.

pastedImage_1.png

pastedImage_2.png

0 Kudos
Reply

3,290 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

and do you also set proper byte length when starting to receive response according schedule list? You have  

LIN_DRV_ReceiveFrameData(INST_LIN1, g_lin_master_Pdu_Matrix[lin_id_index].buf, sizeof( g_lin_master_Pdu_Matrix[lin_id_index].buf));

How this correspond to different byte counts in a schedule list?

BR, Petr

3,290 Views
15736231627
Contributor II

Yes, I corrected this error, and now the schedule set can be received and sent, but I found that there will still be a lot of irrelevant error frames, so I changed the frame gap to 40ms, and there will also be one or two error frames. But I think the frame gap is too long, is there any optimization method?

0 Kudos
Reply

3,290 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try to set higher priority for LPUART interrupt.

Try to rewrite its callback to have faster header response, for example using lin_master_sn and lin_current_ID you updated when header is send, could be ...

 

case LIN_PID_OK:
    /* Set timeout */
    LIN_DRV_SetTimeoutCounter(INST_LIN1, TIMEOUT);

    //if(lin_current_ID == lin1_State->currentId)
    { /* If PID is FRAME_TX_RSP, salve node will receive data from master node */
      if(g_lin_master_schedule_list_config[lin_master_sn].Type == FRAME_RX_RSP )
      {
            /* Call to Receive Frame DATA Function */
            //current_id_sn = lin_id_index;
            //receive_new_frame_flag = 1;
            LIN_DRV_ReceiveFrameData(INST_LIN1, g_lin_master_Pdu_Matrix[lin_master_sn].buf,                   g_lin_master_schedule_list_config[lin_master_sn].len);
            break;
      }
      else if(g_lin_master_schedule_list_config[lin_master_sn].Type == FRAME_TX_RSP)
      {
            /* Call to Send Frame DATA Function */
            LIN_DRV_SendFrameData(INST_LIN1, g_lin_master_Pdu_Matrix[lin_master_sn].buf,                   g_lin_master_schedule_list_config[lin_master_sn].len);
            break;
      }

      else
      {

      }

   }
break;

BR, Petr

0 Kudos
Reply

3,290 Views
15736231627
Contributor II

I find that it's okay to just send a frame, but there will be a problem if you accept a frame to join.

0 Kudos
Reply

3,290 Views
15736231627
Contributor II

I'm using SDK_S32K1XX_15,I dong't have any  errors,In addition, I changed my frame gap, but there was a loss of frames

0 Kudos
Reply

3,290 Views
15736231627
Contributor II

这是我的报文lin.jpg

0 Kudos
Reply

3,290 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

does the issue also happen if you extend time base or increase frame slot duration?

Also when searching for frame ID in lin_rx_tx_handle_callback is the receive (LIN_DRV_ReceiveFrameData) started before slave sends starts sending data?

BR, Petr

0 Kudos
Reply