Why is the data received by LPSPI from the slave out of order?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why is the data received by LPSPI from the slave out of order?

1,716 次查看
kalvin
Contributor I

One of the two MCUs is the master and the other is the slave. The master starts DMA sending/receiving every 5ms and triggers the slave to start DMA receiving/sending through the external interrupt signal (IND).

void MainFunctionRun(void)
{
if(!Task_Delay[0])
{
Task_Delay[0] = 5; //loop every 5ms

SpiMaster_EmitInd(PTE,IND);

DMA_Start(SPI_DMA_RX_CH,SPI_DMA_TX_CH); //master start DMA for spi
}
}

void PORTE_IRQHandler(void)
{
if(((PTE->PDIR >> IND) & 1) == 0) //slave received IND signal
{
DMA_Start(SPI_DMA_RX_CH,SPI_DMA_TX_CH); //slave start DMA for spi
}
else if(((PTE->PDIR >> ACK) & 1) == 0) //no use
{
}
PORTE->ISFR |= (1<<IND)|(1<<ACK);
}

0 项奖励
回复
5 回复数

1,691 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Such effect are usually caused by overflow/underflow condition. How you are triggering DMA transfer on the slave side?

0 项奖励
回复

1,675 次查看
kalvin
Contributor I

In the above code fragment PORTE_IRQHandler, before the master DMA starts, the IND signal will be sent to the slave to trigger the slave DMA reception.

0 项奖励
回复

1,655 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is unusual approach. It is needed to route DMA request directly from LPSPI to DMA module (with using of DMAMUX)

davidtosenovjan_0-1664786751929.png

 

0 项奖励
回复

1,600 次查看
kalvin
Contributor I

@davidtosenovjan any new answers ?

0 项奖励
回复

1,637 次查看
kalvin
Contributor I

I also used DMAMUX @davidtosenovjan .

static void DMAMUX_Init(LPSPI_Type *Instance,uint8_t rxch,uint8_t txch)
{
uint32_t DMA_CH_RX_MUX_NUM = 0; 
if(Instance == LPSPI0) DMA_CH_RX_MUX_NUM = 14;                                //using LPSPI0
if(Instance == LPSPI1) DMA_CH_RX_MUX_NUM = 16;
if(Instance == LPSPI2) DMA_CH_RX_MUX_NUM = 18;

SIM->PLATCGC |= SIM_PLATCGC_CGCDMA(1); 
PCC->PCCn[PCC_DMAMUX_INDEX] |= PCC_PCCn_CGC_MASK; 

/* DMA Channel 4 for LPSPI RX */
DMAMUX->CHCFG[rxch] &= ~ DMAMUX_CHCFG_ENBL(1); 
DMAMUX->CHCFG[rxch] |= DMAMUX_CHCFG_SOURCE(DMA_CH_RX_MUX_NUM); //14
DMAMUX->CHCFG[rxch] |= DMAMUX_CHCFG_ENBL(1); 
/* DMA Channel 5 for LPSPI TX */
DMAMUX->CHCFG[txch] &= ~ DMAMUX_CHCFG_ENBL(1); 
DMAMUX->CHCFG[txch] |= DMAMUX_CHCFG_SOURCE(DMA_CH_RX_MUX_NUM+1); //14+1
DMAMUX->CHCFG[txch] |= DMAMUX_CHCFG_ENBL(1); 
}

0 项奖励
回复