Which Multilink to be used for S32k144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which Multilink to be used for S32k144

316 Views
Dipen
Contributor I

In NXP website it is mentioned PE Micro Multilink Universal supports S32K144, but my supplier says to go with PE Micro Multilink Universal FX. Can I use either of them to program the microcontroller?

0 Kudos
Reply
1 Reply

302 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Dipen,

You can use either of them to program the microcontroller. For more detail, please refer to: Multilink Debug Probes


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply