The file 'S32K1xx_DMA_INT_mapping.xlsm' written on p.117 of 'S32K1xx Series Reference Manual Rev. 14' (S32K-RM.pdf) does not appear in the attachment.
https://community.nxp.com/t5/S32K/about-S32K1xx-DMA-INT-mapping-xlsm/m-p/676527
From this post, it looks like it is attached to the old version, but where can I download the old reference manual?
Hi filu,
I will send you the Rev. 13 S32K-RM. Let me check what's wrong with the latest Rev. 14' S32K1xx Series Reference Manual Rev. 14.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I am running into the same issue. Where can one find S32K1xx_DMA_INT_mapping.xlsm?
Hi @junxi_cai @mks004,
Sorry for the inconvenience we bring you!
Please keep using the S32K1xx_DMA_INT_mapping in Rev13 until the documentation department fixes this issue.
Best Regards,
Robin
Hello Robin,
I have the same issue, could you please also share the S32K-RM REV.13 with me?
Thank you,
Junxi