Using the DDR tool of S32DS 3.5 to verify that there is a problem with DDR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the DDR tool of S32DS 3.5 to verify that there is a problem with DDR

256 Views
WX_H
Contributor I

Hello, I timed out when I used the DDR tool of S32 DS3.5 to generate the DDR parameter. The DDR tool can recognize the serial port and make sure that the string number is correct.The crystal frequency is also 40m.The S32E chip is also running normally, but it is not known that the connection timed out, as shown in the following figure.I look forward to your reply.
Best wishes.

Spoiler
S32E DDR企业微信截图_16848234188230.png

 

Tags (2)
0 Kudos
Reply
0 Replies