Unified bootloader for S32K344

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unified bootloader for S32K344

Jump to solution
11,256 Views
RajaJayaraman
Contributor I

Hi,

I started recently with S32K344 Eval board and would like to know, do you have the Unified bootloader for S32K344 device already ? If not, when it is expected to be released ?

Thanks !

BR
Raja

0 Kudos
Reply
1 Solution
11,240 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Raja,

I just sent you a private massage,

 

Regards,

Daniel

View solution in original post

22 Replies
1,742 Views
JonAnder_Amante
Contributor I

Hi, 

I am using the project "S32K344_Can_bootloader_RTD200" in the microprocessor S32K344. I want to download an application with the program of bootloader. I have achieved the jump from program to application but I have different questions.

1. I want to use #define EN_DELAY_TIME but when I uncomment the command in the folder "public_in", the program has different errors. My target to use "Backdoor", that is to say, I want to check if the program has to enter to bootloader or not. I don´t know the process and the different functions that I have to use to achieve the target. I want to use the function "Boot_CheckReqBootloaderMode(void)" but when I debug the program, it never enters to the "if". Could you explain me the process and the steps to achieve the target. I add different functions that I think are important. 

2. I don´t know if I have to modificate the parameters of "static tJumpAppDelayTimeInfo gs_stJumpAPPDelayTimeInfo = {FALSE, 0u};". I have to change this structure ? You can see all structure in one of the next pictures. 

I need the reply as soon as possible since I have to send a project very soon. 

JonAnder_Amante_0-1713766092310.png

 

 

 

 

JonAnder_Amante_1-1713766092321.png

 

 

 

 

JonAnder_Amante_2-1713766092446.png

 

 

 

 

JonAnder_Amante_3-1713766092473.png

 

 

 

 

JonAnder_Amante_4-1713766092340.png

 

 

 

Thank you for all, 

Jon Ander Amante Jorge

0 Kudos
Reply
9,964 Views
ManoharAher
Contributor I

I am using S32K344  with S32DS 3.4 , S32DS C Compiler Version 10.2.0 and S32k3 RTD 2.0.2  DS2207  but Unified Bootloader V2.0 are not working.

Share the all details and working example.

I have import the example and build but error occurs.

Error:  1) undefined reference to `__INT_SRAM_START' 

           2)  multiple definition of `_start'

0 Kudos
Reply
9,958 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @ManoharAher,

Please create a ticket or a new thread.

 

Thank you

 

0 Kudos
Reply
9,735 Views
ManoharAher
Contributor I
Hi danielmartynek,
 
Please Share the Procedure of S32K344 flash and working from Scratch to end regarding  unified bootloader v2.0 .
 
which file is firstly flash Bootloader or App in on board before start with ECUBUS?
 
I have install ECU BUS software.
 
you have any procedure of Unified Bootloader Demo V2.0.
 
I get the communication  error from ECUBUS " [4908ms][sch1]{"msg":"No response","index":1}"
 
 
 
 
 
 
   
 
 
 
 
0 Kudos
Reply
1,356 Views
JonAnder_Amante
Contributor I

HI, 

I have the same problem and I don´t know how I can solve. Could you tell me the steps to solve the problem?

Thank you for all,

Jon Ander Amante

0 Kudos
Reply
9,952 Views
ManoharAher
Contributor I

Hi danielmartynek,

 

I have already creat the ticket for unified bootloader V2.0 issue.

 

I have attach image of Ticket. 

 

0 Kudos
Reply
9,946 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Thank you,

I see in the ticket that you received an answer from a colleague of mine.

If this does not answer your questions, please update the ticket.

 

BR, Daniel

0 Kudos
Reply
11,241 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Raja,

I just sent you a private massage,

 

Regards,

Daniel

8,390 Views
WangLeiDevelopment
Contributor I

Hi danielmarkynek

 I am develop OTA at S32K344,I also need Unified bootloader demo source code.

0 Kudos
Reply
8,371 Views
danielmartynek
NXP TechSupport
NXP TechSupport
7,792 Views
WangLeiDevelopment
Contributor I

Thanks for you !

But I find Bootloader project(unified_bootloader_demo_V2.1.exe) use C40_IP driver alsways run to hardware Falut . Then I uart for debug ,find program strike at erase and write status function (specific is inside  C40_Ip_Compare function is C40_Ip_SynchronizeCache). I don't know what reason and what should i do.

0 Kudos
Reply
9,963 Views
ManoharAher
Contributor I

Hi danielmartynek

I am using S32K344 with S32DS 3.4 , S32DS C Compiler Version 10.2.0 and S32k3 RTD 2.0.2 DS2207 but Unified Bootloader V2.0 are not working. Share the all details and working example. I have import the example and build but error occurs. Error: 1) undefined reference to `__INT_SRAM_START' 2) multiple definition of `_start'

0 Kudos
Reply
10,279 Views
autolan22
Contributor III

Hi danielmartynek,
I've got some trouble with the bootloader jump to App, Will you please send me a private massage about bootloader demo too? 

thanks,

lan

0 Kudos
Reply
10,274 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi lan,

Please create a ticket or a new thread.

Thank you,

danielmartynek_0-1656420000762.png

 

BR, Daniel

10,611 Views
mattlowe
Contributor I

Hi there,

I'm currently evaluating the S32K344 on RDK344BMU_V20 BMS reference design. Are you able to provide me with the unified bootloader for the S32K344 so I can evaluate this functionality?

Kind regards,

Matt

0 Kudos
Reply
10,594 Views
RajaJayaraman
Contributor I

Hi Matt,

I have not received the bootloader from NXP yet, we should ask this question to NXP.

Best regards,

Raja

0 Kudos
Reply
10,580 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @RajaJayaraman, @mattlowe,

I'm sorry for the delay.

We don't get notifications for updates in old threads,

Please create a ticket.

danielmartynek_0-1646920221941.png

 

BR, Daniel

 

10,786 Views
tianxing
Contributor III

HI,I need a it too.

Can you send me a copy ?

0 Kudos
Reply
10,760 Views
RajaJayaraman
Contributor I

Hi,

It was due for release in April but I did not get this bootloader from NXP until now.

BR
Raja

0 Kudos
Reply
10,959 Views
jacst
Contributor II

Hello. I need it too, can you release a copy for me?

0 Kudos
Reply