Hi,
I am facing issues running the Hello World (S32K148_Project_Hello without SDK) from the example projects provided with S32 Design Studio. I built my project and set the debug configurations with an OpenSDA USB port as in interface. However, when I try to set the run configurations and run my project I get the following error:
Error starting process.
Cannot run program "C:\Users\vinam\Desktop\S32K\Projects\S32K148_Project_Hello\Debug\S32K148_Project_Hello.elf": Launching failed
I believe there is some issue with the .elf generated while building the project, but I do not know how to resolve it.
Kind regards,
Hi,
are you running PE Micro debug probe based session given in this example?
I have no issue with that demo example.
BR, Petr
Hi Petr,
Yes, I am running the PE micro debug probe. I have no issues running the project in debug mode, however, I cannot run the project after setting run configurations:
When I try to run the project, I get the error I mentioned before.
Regards,
Hi,
Run C/C++ application means execute it on Windows machine. This approach is impossible with binary built for ARM M4 core.