UJA1169ATK3 timing latency.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UJA1169ATK3 timing latency.

1,761 Views
sambath_kumar_k
Contributor I

We are using UJA1169ATK3 and would like to know certain timing specification.

  • * Time taken for switching between modes of SBC like from Power off to RESET to Standby,
  • * Time taken  from Standby mode to Normal mode and from Normal mode to Standby mode after it is configured to the respective mode via SPI communication or reset.
  • * What would be the state of CAN line, RST pin, Limp, Watchdog and any other specific changes during the transition time(Normal to standby ).
  • * What would be the state of CAN line, RST pin, Limp, Watchdog and any other specific changes during the transition time(standby to normal ).
  • * I was able to see, that startup(CAN) in datasheet, I assume that this is the time taken for CAN to be able to communicate from the instant CAN is configured to be in active mode after SBC is configured to Normal mode. We will not be using the SBC sleep mode or the wake up functionality of CAN. Please provide clarifications for the above.
0 Kudos
Reply
3 Replies

1,718 Views
guoweisun
NXP TechSupport
NXP TechSupport

Had replied to your based on case00297372

0 Kudos
Reply

1,718 Views
sambath_kumar_k
Contributor I

I see something like this

When I click, It is taking to a new website where it asks for login id and password and failed.

Can you please help me the answer for my questions.

Thank you,

Kardhik Sambathkumar

Platform Software

Integrated Components and Solutions(ICS)

Caterpillar: Confidential Green

0 Kudos
Reply

1,718 Views
sambath_kumar_k
Contributor I

I cannot view the answer

0 Kudos
Reply