Hi,
I couldn`t find any example project for Tresos. I have download several MCAL versions to check this. Inside of installation folder for MCALs(C:\NXP\AUTOSAR\S32K1XX_MCAL4_0_RTM_1_0_5) there is no example project. Only the plugins available.
It is same situation for RTD, it has only plugins there is no example. How can I find the Tresos example for S32K148?
Solved! Go to Solution.
Hello,
Sample application are for example in S32K14X_MCAL4_0_RTM_1_0_4 and there are correct versions.
If you want to use 1.0.0 you will need to replace it with correct version. (0.9.0. in this case) - I didn't seen it available.
The examples for SW32K1_RTD_4.4_1.0.1 are located in:
:\NXP\SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples\EBT\Adc_example_S32K148
Similar in folders for each driver.
For the beginning I would recommend to use RTD (real time drivers) instead of MCAL.
There are much more examples.
Best regards,
Peter
Hello,
Hmm, that is strange.
I have just installed version S32K14Xx_MCAL4_0_RTM_1_0_0 and sample application is there:
Usually the sample applications are in the base releases.
Best regards,
Peter
Hi Peter,
Thank you for the answer. Yes sample application is only available in base version. but now I have a problem while opening the project in Tresos. sample project uses "xxx_TS_T40D2M9I0R0" version plugins but I have "xxx_TS_T40D2M10I0R0" with base version. It seems that sample project is using older version. Do you know where can I find this version?
Best regards
Hello,
Sample application are for example in S32K14X_MCAL4_0_RTM_1_0_4 and there are correct versions.
If you want to use 1.0.0 you will need to replace it with correct version. (0.9.0. in this case) - I didn't seen it available.
The examples for SW32K1_RTD_4.4_1.0.1 are located in:
:\NXP\SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples\EBT\Adc_example_S32K148
Similar in folders for each driver.
For the beginning I would recommend to use RTD (real time drivers) instead of MCAL.
There are much more examples.
Best regards,
Peter